This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

材料有限,这样连接USB可以吗?



材料有限,这样连接USB可以吗?不是做产品,因为不在实验室,自己买的材料非常非常不足,只是想试一下MSP430的USB而已.

PUR好像就是为了BSL,如果我不要BSL,是不是可以这样.

图中的两个R8(忘了编号,应该都是一样功能的吧.),可以选择范围是多少.我的0.1uF是104独石电容.