This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用msp430f5系列开启25M的高速内部时钟时出现的问题

Other Parts Discussed in Thread: MSP430F5529

能否帮我看下这个官方例程?
这个例程可以开启25M的主时钟,但是我确实很多地方都看不懂啊,谁能帮我解释一下呢?主要是

void SetVcoreUp (unsigned int level)这个函数不懂,学1系列的时候,这里面的东西压根没见过,他们有什么作用?为什么要对他们进行设置?我试了其他可以开启25M的程序,结果发现,程序运行时他们都跑飞了,就这个程序可以开启。是不是

void SetVcoreUp (unsigned int level)可以防止跑飞啊?谢谢啊~

程序如下:

#include <msp430f5529.h>

void SetVcoreUp (unsigned int level)

{          

 // Open PMM registers for write

 PMMCTL0_H = PMMPW_H;              

 // Set SVS/SVM high side new level

 SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level;

 // Set SVM low side to new level

 SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level;

 // Wait till SVM is settled

 while ((PMMIFG & SVSMLDLYIFG) == 0);

 // Clear already set flags

 PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);

 // Set VCore to new level

 PMMCTL0_L = PMMCOREV0 * level;

 // Wait till new level reached

 if ((PMMIFG & SVMLIFG))

   while ((PMMIFG & SVMLVLRIFG) == 0);

 // Set SVS/SVM low side to new level

 SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level;

 // Lock PMM registers for write access

 PMMCTL0_H = 0x00;

}

void TIME(void)

{

 SetVcoreUp (0x01);

 SetVcoreUp (0x02);  

 SetVcoreUp (0x03);  

  UCSCTL3 = SELREF_2;                       // Set DCO FLL reference = REFO

 UCSCTL4 |= SELA_2;                        // Set ACLK = REFO

__bis_SR_register(SCG0);                  // Disable the FLL control loop

 UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx

 UCSCTL1 = DCORSEL_7;                      // Select DCO range 50MHz operation

 UCSCTL2 = FLLD_1 + 762;                  // Set DCO Multiplier for 25MHz

                                           // (N + 1) * FLLRef = Fdco// (762 + 1) * 32768 = 25MHz // Set FLL Div = fDCOCLK/2

 __bic_SR_register(SCG0);                  // Enable the FLL control loop

 // Worst-case settling time for the DCO when the DCO range bits have been

 // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx

 // UG for optimization.

 // 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle

 __delay_cycles(782000);

 // Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize

 do

 {

   UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);

                                           // Clear XT2,XT1,DCO fault flags

   SFRIFG1 &= ~OFIFG;                      // Clear fault flags

 }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag

 

 __no_operation(); //设断点观察时钟输出引脚上的波形和频率

 

 

// P3OUT|=BIT0;

 

}

 

能否帮我看下这个官方例程?
这个例程可以开启25M的主时钟,但是我确实很多地方都看不懂啊,谁能帮我解释一下呢?主要是

void SetVcoreUp (unsigned int level)这个函数不懂,学1系列的时候,这里面的东西压根没见过,他们有什么作用?为什么要对他们进行设置?我试了其他可以开启25M的程序,结果发现,程序运行时他们都跑飞了,就这个程序可以开启。是不是

void SetVcoreUp (unsigned int level)可以防止跑飞啊?谢谢啊~

程序如下:

#include <msp430f5529.h>

void SetVcoreUp (unsigned int level)

{          

 // Open PMM registers for write

 PMMCTL0_H = PMMPW_H;              

 // Set SVS/SVM high side new level

 SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level;

 // Set SVM low side to new level

 SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level;

 // Wait till SVM is settled

 while ((PMMIFG & SVSMLDLYIFG) == 0);

 // Clear already set flags

 PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);

 // Set VCore to new level

 PMMCTL0_L = PMMCOREV0 * level;

 // Wait till new level reached

 if ((PMMIFG & SVMLIFG))

   while ((PMMIFG & SVMLVLRIFG) == 0);

 // Set SVS/SVM low side to new level

 SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level;

 // Lock PMM registers for write access

 PMMCTL0_H = 0x00;

}

void TIME(void)

{

 SetVcoreUp (0x01);

 SetVcoreUp (0x02);  

 SetVcoreUp (0x03);  

  UCSCTL3 = SELREF_2;                       // Set DCO FLL reference = REFO

 UCSCTL4 |= SELA_2;                        // Set ACLK = REFO

__bis_SR_register(SCG0);                  // Disable the FLL control loop

 UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx

 UCSCTL1 = DCORSEL_7;                      // Select DCO range 50MHz operation

 UCSCTL2 = FLLD_1 + 762;                  // Set DCO Multiplier for 25MHz

                                           // (N + 1) * FLLRef = Fdco// (762 + 1) * 32768 = 25MHz // Set FLL Div = fDCOCLK/2

 __bic_SR_register(SCG0);                  // Enable the FLL control loop

 // Worst-case settling time for the DCO when the DCO range bits have been

 // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx

 // UG for optimization.

 // 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle

 __delay_cycles(782000);

 // Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize

 do

 {

   UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);

                                           // Clear XT2,XT1,DCO fault flags

   SFRIFG1 &= ~OFIFG;                      // Clear fault flags

 }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag

 

 __no_operation(); //设断点观察时钟输出引脚上的波形和频率

 

 

// P3OUT|=BIT0;

 

}

 

能否帮我看下这个官方例程?

这个例程可以开启25M的主时钟,但是我确实很多地方都看不懂啊,谁能帮我解释一下呢?主要是

void SetVcoreUp (unsigned int level)这个函数不懂,学1系列的时候,这里面的东西压根没见过,他们有什么作用?为什么要对他们进行设置?我试了其他可以开启25M的程序,结果发现,程序运行时他们都跑飞了,就这个程序可以开启。是不是

void SetVcoreUp (unsigned int level)可以防止跑飞啊?谢谢啊~

程序如下:

#include <msp430f5529.h>
void SetVcoreUp (unsigned int level)
{          
  // Open PMM registers for write
  PMMCTL0_H = PMMPW_H;             
  // Set SVS/SVM high side new level
  SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level;
  // Set SVM low side to new level
  SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level;
  // Wait till SVM is settled
  while ((PMMIFG & SVSMLDLYIFG) == 0);
  // Clear already set flags
  PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);
  // Set VCore to new level
  PMMCTL0_L = PMMCOREV0 * level;
  // Wait till new level reached
  if ((PMMIFG & SVMLIFG))
    while ((PMMIFG & SVMLVLRIFG) == 0);
  // Set SVS/SVM low side to new level
  SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level;
  // Lock PMM registers for write access
  PMMCTL0_H = 0x00;
}
void TIME(void)
{
  SetVcoreUp (0x01);
  SetVcoreUp (0x02); 
  SetVcoreUp (0x03); 
   UCSCTL3 = SELREF_2;                       // Set DCO FLL reference = REFO
  UCSCTL4 |= SELA_2;                        // Set ACLK = REFO
__bis_SR_register(SCG0);                  // Disable the FLL control loop
  UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx
  UCSCTL1 = DCORSEL_7;                      // Select DCO range 50MHz operation
  UCSCTL2 = FLLD_1 + 762;                   // Set DCO Multiplier for 25MHz
                                            // (N + 1) * FLLRef = Fdco// (762 + 1) * 32768 = 25MHz // Set FLL Div = fDCOCLK/2
  __bic_SR_register(SCG0);                  // Enable the FLL control loop
 
  // Worst-case settling time for the DCO when the DCO range bits have been
  // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
  // UG for optimization.
  // 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle
  __delay_cycles(782000);
 
  // Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
  do
  {
    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
                                            // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG;                      // Clear fault flags
  }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag
 
  __no_operation(); //设断点观察时钟输出引脚上的波形和频率
 
 
// P3OUT|=BIT0;
 
}