This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
查看过MSP430F551x_552x数据手册,只找到参数RI Input MUX ON resistance 0V≤VAx≤AVCC 10(min) 200(typ) 1900 Ω(max),page:70/122,输入选择器导通电阻,这个和ADC的输入阻抗有什么关系?
我想用MSP430F5529的一个ADC采集信号,信号3.8V经过2个4.7M的电阻分压,ADC的输入阻抗参数如果远大于4.7M将不会有什么影响,若输入阻抗与4.7M相当或远小于4.7M信号分压比将会受到影响。不知道ADC的输入阻抗多大?分压电阻值参数是否合理?(分压电阻不宜过小)。谢谢!
您好!我的采样电压范围0V~4.2V(直流),想用精密电阻分压,分压电阻27K+100K是否合理?或给予推荐电阻值(论坛中相关的两个帖子查看过。)
MSP430的ADC输入阻抗有没有具体的参考参数?先确定硬件电路设计,然后完善采样保持时间的软件控制方法。谢谢!