Part Number: MSP430F5438A

如这段描述,LPM0 through LPM4是通过设置SR寄存器中的CPUOFF, OSCOFF, SCG0, and SCG1位实现不同的低功耗模式的

从这张图看,LPM模式应该不会影响SMCLK的吧?如果XT2在电路上配置了一个高频晶体,并且将SMCLK的源设置为XT2
LPM3会影响SMCLK吗?进入LPM3,会将SMCLKOFF进行相应的设置从而关闭SMCLK吗

我用CCS进行调试,使用5438A头文件中定义的LPM3使单片机进入低功耗模式,但是我在这条语句的定义中并没有看到操作SMCLKOFF,但是Table1-2的描述中LPM3
下SMCLK是disable的,这是怎么实现的呢