This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12CLK = SMCLK = 5MHz时的寄存器设置



我想用DCO + FLL来得到较为稳定的5MHz,所以设置了一下寄存器:

{

P5SEL |= BIT4 + BIT5;              // Port select XT1
REFCTL0 &= ~REFMSTR;

UCSCTL6 &= ~(XT1OFF);       // XT1 On
UCSCTL6 |= XCAP_3;             // Internal load cap

// Loop until XT1 fault flag is cleared
do
{
UCSCTL7 &= ~XT1LFOFFG;            // Clear XT1 fault flags
}while (UCSCTL7&XT1LFOFFG);    // Test XT1 fault flag

// Initialize DCO to 5MHz
__bis_SR_register(SCG0);              // Disable the FLL control loop

UCSCTL0 = 0x0000;                          // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_5;               // 2.5MHz - 6MHz
UCSCTL2 = FLLD_0 + 152;             // Set DCO Multiplier for 5MHz
                                                               // (N + 1) * FLLRef = Fdco
                                                               // (152 + 1) * 32768 = 5MHz
                                                               // Set FLL Div = fDCOCLK/1
UCSCTL3 = SELREF_2 + FLLREFDIV_0;
UCSCTL4 = SELA_0 + SELS_3 + SELM_3;
UCSCTL5 = DIVPA_0 + DIVA_0 + DIVS_0 + DIVM_0;

__bic_SR_register(SCG0);             // Enable the FLL control loop

// 32 x 32 x 5 MHz / 32,768 Hz = 156250= MCLK cycles for DCO to settle
__delay_cycles(156250);

}
这样的设置是不是有问题啊?多谢
  • 你好!

    下面这一段代码是将XT1的32768HZ倍频到2MHZ的示例,请参考。

    // Configuration: XT1 = 32768HZ, ACLK = 32768HZ, MCLK = SMCLK = 2MHz

    UCSCTL2 = FLLD_0 + FLLN5_L + FLLN4_L + FLLN3_L + FLLN2_L ; // FLL output = XT1CLK * 61
    UCSCTL3 = SELREF__XT1CLK; // Select XTCLK as the FLL source
    UCSCTL4 = SELA__XT1CLK + SELS__DCOCLK + SELM__DCOCLK; // ACLK = XT1CLK, MCLK = SMCLK = DCOCLK
    UCSCTL6 = XT2OFF + XT1DRIVE_0 + XCAP_3; // XT2OFF, XCAP 12pf
    UCSCTL6 &= ~XT1OFF; // XT1ON