最近一直在调试430的串口问题,在调试过程中出现这样的问题,将单片机的串口引脚TXD和RXD悬空,功耗特别的大,实验测得的功耗为61uA,但是如果将串口引脚RXD和TXD直接连上RS232的TXD和RXD时,这时候功耗一下就下来了,降到了0.5uA。(附注:对于单片机的未用引脚全部都设为上拉输入,P1.1设为串口输入,P1.2设置为串口输出)。现在一直被这问题困扰着,想请教下各位大虾帮忙给解释下,谢谢!下面附上我的MSP430单片机的串口连接图。
图中的网络标号MRXD连接到单片机的RXD引脚,MTXD连接到单片机的TXD引脚。图中的网络标号RXD和TXD为系统对外的接口。UU_D3、UU_D4、UU_D5为6V的TVRS管(SMBJ6.0CA)。