This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于msp430驱动LCD

Other Parts Discussed in Thread: MSP430F427A

用MSP430F427A 驱动LCD   选择分压电阻100k,用示波器看COM口和S0~S11 都能看到波形,但是液晶屏就是无显示   求指导
#include <msp430x42x.h>

#define uint unsigned int
#define uchar unsigned char
#define ulong unsigned long

//************* 延时定义***************************
#define CPU_F ((double)32768.0)
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))
#define dealy_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))

//******************LCD码表************************
uchar const duanma[]={
  0x7d,    //0
  0x60,    //1
  0x3e,    //2
  0x7a,    //3
  0x63,    //4
  0x5b,    //5
  0x5f,    //6
  0x70,    //7
  0x7f,    //8
  0x7b     //9
};
uchar i,j;


void main()
{
  WDTCTL = WDTPW+WDTHOLD;
  BTCTL=BT_fLCD_1K+BT_fCLK2_ACLK;
//  clock_init();

  LCDCTL=LCDSG0_1+LCD4MUX+LCDON;


  uchar i;


  while(1)
  {
    for(i=0;i<5;i++)
    {
      LCDMEM[i]=duanma[i];
    }
  
  }
}

  • 如果你确保你所有的硬件都没有问题,这个代码有一个缺陷,就是没有设置LCD的时钟设置的1K,会不会是因为频率太高了,造成眼睛看不到。

    代码上看不到其他问题。

  • 屏幕上可以显示很淡的字,我试过别的频率,基本上屏上没有什么变化,只是侧着屏幕看,能看见一点,那几个电阻我改为820k,一样是很淡的,你的QQ或者别的联系方式能给我一下么?

  • 屏幕上可以显示很淡的字,我试过别的频率,基本上屏上没有什么变化,只是侧着屏幕看,能看见一点,那几个电阻我改为820k,一样是很淡的,你的QQ或者别的联系方式能给我一下么?

  • 确定下你的LCD的工作电压范围,一般的LCD有5.0V和3.3V两种工作范围,如果你用的5V的LCD就可能出现你所描述的情况。