Other Parts Discussed in Thread: MSP430F427A
用MSP430F427A 驱动LCD 选择分压电阻100k,用示波器看COM口和S0~S11 都能看到波形,但是液晶屏就是无显示 求指导
#include <msp430x42x.h>
#define uint unsigned int
#define uchar unsigned char
#define ulong unsigned long
//************* 延时定义***************************
#define CPU_F ((double)32768.0)
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))
#define dealy_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))
//******************LCD码表************************
uchar const duanma[]={
0x7d, //0
0x60, //1
0x3e, //2
0x7a, //3
0x63, //4
0x5b, //5
0x5f, //6
0x70, //7
0x7f, //8
0x7b //9
};
uchar i,j;
void main()
{
WDTCTL = WDTPW+WDTHOLD;
BTCTL=BT_fLCD_1K+BT_fCLK2_ACLK;
// clock_init();
LCDCTL=LCDSG0_1+LCD4MUX+LCDON;
uchar i;
while(1)
{
for(i=0;i<5;i++)
{
LCDMEM[i]=duanma[i];
}
}
}