This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于G2系列,请问datasheet开头的特征介绍这个External Digital Clock Source具体怎么理解?
我在引脚说明中好像没有找到关于这个的输入端,如果仅仅是定时器之类的时钟输入的话,那么为什么在MSP430x2xx Family User's Guide (Rev. I)slau144i第281页这样写道:
LFXT1 may be used with an external clock signal on the XIN pin in either LF or HF mode when
LFXT1Sx = 11, OSCOFF = 0, and XCAPx = 00. When used with an external signal, the external
frequency must meet the data sheet parameters for the chosen mode. When the input frequency is below
the specified lower limit, the LFXT1OF bit may be set preventing the CPU from being clocked with
LFXT1CLK.
这个又怎么理解呢?在哪里为引脚输入端?
如果G2系列没有此功能,为什么在第290页中关于LFXT1Sx的配置中没有标明适合哪些系列器件呢?
LFXT1Sx Bits 5-4 Low-frequency clock select and LFXT1 range select. These bits select between LFXT1 and VLO when XTS =
0, and select the frequency range for LFXT1 when XTS = 1.
When XTS = 0:
00 32768-Hz crystal on LFXT1
01 Reserved
10 VLOCLK (Reserved in MSP430F21x1 devices)
11 Digital external clock source
也许手册其它地方有说明,这里问一下省得自己因为粗心花许多时间仔细寻找,烦请哪位指点一下。如果能总结写一下External Digital Clock Source使用方法和注意事项,那就更感谢了。
谢谢
External Digital Clock Source的含义,就是允许外接一个数字clock 信号给MCU用作振荡源。它和接晶振的区别是晶振还需要内部的激励信号让晶振起振,而外界clock信号是不需要的。
关于这个信号的输入引脚,User Guide上写得很清楚啊,就是XIN。“LFXT1 may be used with an external clock signal on the XIN pin"。对G2xx系列而言,需要把XIN所在GPIO的第二功能选择打开。另外和所允许晶振的震荡范围相同,G2xx系列的External Digital Clock Srouce一样不能接高频的clock,在datasheet上有说明,最高只能接50K。
实在不好意思,又看漏眼了
不过datasheet的引脚表是不是确实没有明确注明呀
User Guide注明了用XIN引脚输入,在Datasheet上Terminal Function上应该就不会在解释了,因为External Digital Clock Resource有点被归为XIN的功能了。