This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
基本流程就是通过CCS6.0生成HEX文件载入Proteus进行仿真
首先,这是仿真图,用P2口控制8个LED灯的熄灭
核心代码如下:
#pragma vector = TIMERA0_VECTOR __interrupt void timer_A(void) { P2OUT = (0x01u << 0); }
P2输出造成第0盏灯亮
上面是仿真结果,这没什么问题,然后将代码修改如下:
#pragma vector = TIMERA0_VECTOR __interrupt void timer_A(void) { unsigned int order = 0; P2OUT = (0x01u << order); }
理论上,仿真结果应该没有任何变化才对,但是实际结果是这个:
如图,D2亮,想了好久实在想不通为什么,最有可能的就是CCS6.0编译成HEX文件的时候出现了问题,或者是我的配置问题?
使用IAR来编译完全没有问题,已试。