This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我在使用MSP430F6638 使用CCS5 无法烧录程序

Other Parts Discussed in Thread: MSP430F6638, MSP-EXP430F5529LP

我在使用MSP430F6638 使用CCS5 无法烧录程序

MSP430: Trouble Writing Memory Block at 0x8000 on Page 0 of Length 0x22: Could not erase device memory
MSP430: GEL: File: F:\EE\TI\workspace\LED_test1\Debug\LED_test1.out: Load failed.

我曾经在同一台电脑,同一块板子上下载烧录过,但是现在再也无法烧录。并一直是这个error

我室友的板子是DY-FFTB6638

  •        MSP430的CMD文件都在CCS的安装文件下面找得到,一般在建立工程的时候,你选择了相关的device就会自动产生相对应的cmd文件了。

    你可以确定一下你的CCS project的属性没有做任何的变化。另外可以尝试先clear project,然后在rebuild一下看看。

  • 我clean也rebuild了依旧没用。

    我今天晚上刚才还可以烧录(我没有做任何改变,重装了CCS5.4,就可以烧录了),

    但是就五分钟前,我同一个程序,同一台电脑,同一台MSP试验箱,我甚至都没有重启,就发生了同样不能烧录的问题。

    CCS 实在是太不稳定了。唉~~~~

    MSP430: Trouble Writing Memory Block at 0x8000 on Page 0 of Length 0x13c: Could not erase device memory
    MSP430: GEL: File: F:\EE\TI\msp430fftb6638v3.0\MSP430F6638_DemoV3.0\15.LCD_segment\MSP430F6638_SegmentLCD\Debug\MSP430F6638_SegmentLCD.out: Load failed.

  • 我之前装了CCS3.3,烧写不进去,换了5.5,一次性成功烧写。我用 都是MSP-EXP430F5529LP .

  • 建议使用较新版本的ccs。

    一般新版本支持的msp430型号更全,功能更完善