This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用MSP430F6638 使用CCS5 无法烧录程序
MSP430: Trouble Writing Memory Block at 0x8000 on Page 0 of Length 0x22: Could not erase device memory
MSP430: GEL: File: F:\EE\TI\workspace\LED_test1\Debug\LED_test1.out: Load failed.
我曾经在同一台电脑,同一块板子上下载烧录过,但是现在再也无法烧录。并一直是这个error
我室友的板子是DY-FFTB6638
我clean也rebuild了依旧没用。
我今天晚上刚才还可以烧录(我没有做任何改变,重装了CCS5.4,就可以烧录了),
但是就五分钟前,我同一个程序,同一台电脑,同一台MSP试验箱,我甚至都没有重启,就发生了同样不能烧录的问题。
CCS 实在是太不稳定了。唉~~~~
MSP430: Trouble Writing Memory Block at 0x8000 on Page 0 of Length 0x13c: Could not erase device memory
MSP430: GEL: File: F:\EE\TI\msp430fftb6638v3.0\MSP430F6638_DemoV3.0\15.LCD_segment\MSP430F6638_SegmentLCD\Debug\MSP430F6638_SegmentLCD.out: Load failed.