我用的是MSP430F5529,然后我看他的手册上说的是最高可以倍频到135MHZ(DCO FLL倍频),我想问一下的是如果我倍频到这么高会对哪些模块有影响,或者在不影响这些模块的情况下,最高设置成几兆?25M吗?我想让他做四轴的主控芯片,25M够吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的是MSP430F5529,然后我看他的手册上说的是最高可以倍频到135MHZ(DCO FLL倍频),我想问一下的是如果我倍频到这么高会对哪些模块有影响,或者在不影响这些模块的情况下,最高设置成几兆?25M吗?我想让他做四轴的主控芯片,25M够吗?
按照数据手册,MCLK只能跑到25MHz (当然,一定范围内的超频是允许的,但是不建议这么做,当你倍频超过系统承受的频率的时候,系统是不能正常工作的。), 但是时钟系统的外部晶体输入可以支持高达32MHz, FLL控制的DCO输出最高可达135MHz, 但是CPU的MCLK的时钟源无论是从DCO,XT1还是XT2来,分频后最好降到25Mhz以下。
其他模块可以使用的时钟源一般不会超过系统时钟,即不会超过主频,具体参数参见数据手册。