This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: I2CSLAVE__EUSCI_VECTOR中断在传输什么数据?

Part Number: MSP430FR6043

使用的例程是MSP430FR6043EVM_USS_Water_Demo,单步调试的时候跳到了common->DesignCenter->comm->drivers->i2cslave.c中的I2CSLAVE__EUSCI_VECTOR中断,看不懂这个中断在传输什么数据。

#pragma vector=I2CSLAVE__EUSCI_VECTOR
__interrupt void I2CSlave_ISR(void)
{
	uint8_t ui8Data;
    uint16_t u16Temp;

	switch (__even_in_range(I2CSLAVE__EUSCI_IV, USCI_I2C_UCTXIFG0))
	{
		case USCI_I2C_UCSTTIFG:
			//
			// Check for the repeated start case.  If this is a repeated start
			// and the previous operation was a write to this device,
			// handle the written (received) data.  If this is a first-time stard,
			// the previous I2C state is eI2CSlaveIsIdle.
			//
			if (g_I2CSlaveStatus == eI2CSlaveIsBeingWrittenTo)
			{
				if (I2CSlave_handleEndOfReceive() == true)
				{
					__bic_SR_register_on_exit(I2CSLAVE__LPMx_bits);
				}
			}

			//
			// Reset the I2C Index to zero to begin the new transaction.
			// Then check the I2C mode (read/write) to determine
			// the transaction mode.
			//
			g_ui16I2CIndex = 0;
			if (EUSCI_B_I2C_getMode(I2CSLAVE__EUSCI_B_PERIPHERAL)
					== EUSCI_B_I2C_TRANSMIT_MODE)
			{
				//
				// If this is a read operation (read from this device),
				// cancel the slave request flag and trigger and active
				// exit to alert the application that the flag has changed.
				//
				g_I2CSlaveStatus = eI2CSlaveIsBeingRead;
				g_bI2CSlaveRequestPending = false;
				__bic_SR_register_on_exit(I2CSLAVE__LPMx_bits);

				//
				// If the driver is set up to send the number of bytes to be read
				// before the rest of the buffer, load the number as the first data byte.
				// Otherwise, load the first byte of the transmit buffer into the peripheral.
				//
				if (g_pI2CSlavePort->bSendReadLengthFirst == true)
				{
					ui8Data = g_ui16I2CLength;
				}
				else
				{
					ui8Data = g_pI2CTransmitBuffer[g_ui16I2CIndex++];
				}
				EUSCI_B_I2C_slavePutData(
						I2CSLAVE__EUSCI_B_PERIPHERAL,
						ui8Data
					);
			}
			else
			{
				//
				// If this is a write operation (write from master to this device),
				// update the status accordingly and continue (no additional action is necessary).
				//
				g_I2CSlaveStatus = eI2CSlaveIsBeingWrittenTo;
			}

			//
			// If the slave timeout feature is enabled, schedule a
			// transaction timeout.
			//
#if (I2CSLAVE__TIMEOUT_ENABLE==true)
			Timer_scheduleDelayedFunction(eTimerDelayedFunction_B);
#endif /* I2CSLAVE__TIMEOUT_ENABLE==true */
			break;

		case USCI_I2C_UCSTPIFG:
			//
			// If the timeout feature is enabled, cancel
			// the transaction timeout as the operation
			// has finished successfully.
			//
#if (I2CSLAVE__TIMEOUT_ENABLE==true)
			Timer_cancelDelayedFunction(eTimerDelayedFunction_B);
#endif /* I2CSLAVE__TIMEOUT_ENABLE==true */


			if (g_I2CSlaveStatus == eI2CSlaveIsBeingWrittenTo)
			{
				//
				// If the operation that is ending was a write to this
				// device, handle the written (received) data, and exit
				// active if the callback function requested it.
				//
				if (I2CSlave_handleEndOfReceive() == true)
				{
					__bic_SR_register_on_exit(I2CSLAVE__LPMx_bits);
				}
			}
			else if (g_I2CSlaveStatus == eI2CSlaveIsBeingRead)
			{
				//
				// If the opreation that is ending was a read from this device,
				// exit active in case a transmit (read) buffer pointer update
				// was pending upon this read.
				//
				__bic_SR_register_on_exit(I2CSLAVE__LPMx_bits);
			}

			//
			// Set new status to idle, as the I2C transaction has stopped.
			//
			g_I2CSlaveStatus = eI2CSlaveIsIdle;
			break;

		case USCI_I2C_UCRXIFG0:
			//
			// Grab the received (written) byte from the I2C peripheral.
			// If there is receive buffer space left, store the received
			// byte in the receive buffer.  Otherwise, discard it and call
			// the error callback fxn if one is registered.
			//
			ui8Data = EUSCI_B_I2C_slaveGetData(I2CSLAVE__EUSCI_B_PERIPHERAL);
			if (g_ui16I2CIndex < g_pI2CSlavePort->ui16ReceiveBufferSize)
			{
				g_pI2CSlavePort->pReceiveBuffer[g_ui16I2CIndex++] = ui8Data;
			}
			else
			{
				if (g_pI2CSlavePort->pvErrorCallback != 0)
				{
					g_pI2CSlavePort->pvErrorCallback(eI2CSlaveReceiveBufferFull);
				}
			}
			break;

		case USCI_I2C_UCTXIFG0:
			//
			// If the transmit index is less than the length, there is still
			// valid data in the buffer.  Load the next byte.
			// Else, there is no valid data left in the buffer, so transmit
			// the invalid byte.
			//
            u16Temp = g_ui16I2CLength;
			if (g_ui16I2CIndex<u16Temp)
			{
				ui8Data = g_pI2CTransmitBuffer[g_ui16I2CIndex++];
			}
			else
			{
				ui8Data = I2CSLAVE__INVALID_BYTE;
				if (g_pI2CSlavePort->pvErrorCallback != 0)
				{
					g_pI2CSlavePort->pvErrorCallback(eI2CSlaveWasReadBeyondTransmitBuffer);
				}
			}
			EUSCI_B_I2C_slavePutData(I2CSLAVE__EUSCI_B_PERIPHERAL, ui8Data);
			break;
	}
}

#endif /* I2CSLAVE__ENABLE==true */