Part Number: MSP430FR2476
您好:
我使用IEC60730的SDK进行FRAM的CRC检测,我看到提供的CRC接口如下所示,请问下,我的.text.2的起始地址是0x10000,如果我想诊断这里的代码,我应该怎么做?
static uint16_t privateCalculateCRC(uint16_t *pStartAddress, uint16_t memorySize){
uint32_t i;
// Feed WDT in case user has WDT enabled before running CRC test
#if ENABLED_WDT
uint16_t wdtConfig = WDTCTL & 0x00ff;
WDTCTL = WDTPW + WDTCNTCL + wdtConfig;
#endif // ENABLED_WDT
// If MSP430 has a CRC module, checksum is calculated using CRC module
#if defined(__MSP430_HAS_CRC__)
// Set initial value for CRC16-CCITT calculation
CRCINIRES= CRC16_CCITT_SEED;
for (i = 0; i < memorySize/2; i++)
{
//Add all of the values into the CRC signature
CRCDIRB= *pStartAddress++;
// Feed WDT in case user has WDT enabled before running CRC test
#if ENABLED_WDT
if((i%50)==0)
{
WDTCTL = WDTPW + WDTCNTCL + wdtConfig;
}
#endif // ENABLED_WDT
}
return (CRCINIRES);
#else
uint8_t j;
uint16_t memoryContent;
uint16_t crc = CRC16_CCITT_SEED;
for(i = 0 ; i < memorySize/2 ; i ++)
{
// Byte reverse
memoryContent = ((*pStartAddress & 0x00FF) << 8) +
((*pStartAddress & 0xFF00) >> 8);
for(j = 0 ; j < 16 ; j++)
{
if((memoryContent ^ crc) >> 15){
crc = (crc << 1) ^ CRC16_CCITT_POLY;
}else{
crc <<= 1;
}
memoryContent <<= 1;
}
pStartAddress++;
}
return crc;
#endif //__MSP430_HAS_CRC__
}