您好:
我使用IEC60730的SDK进行FRAM的CRC检测,我看到提供的CRC接口如下所示,请问下,我的.text.2的起始地址是0x10000,如果我想诊断这里的代码,我应该怎么做?
static uint16_t privateCalculateCRC(uint16_t *pStartAddress, uint16_t memorySize){ uint32_t i; // Feed WDT in case user has WDT enabled before running CRC test #if ENABLED_WDT uint16_t wdtConfig = WDTCTL & 0x00ff; WDTCTL = WDTPW + WDTCNTCL + wdtConfig; #endif // ENABLED_WDT // If MSP430 has a CRC module, checksum is calculated using CRC module #if defined(__MSP430_HAS_CRC__) // Set initial value for CRC16-CCITT calculation CRCINIRES= CRC16_CCITT_SEED; for (i = 0; i < memorySize/2; i++) { //Add all of the values into the CRC signature CRCDIRB= *pStartAddress++; // Feed WDT in case user has WDT enabled before running CRC test #if ENABLED_WDT if((i%50)==0) { WDTCTL = WDTPW + WDTCNTCL + wdtConfig; } #endif // ENABLED_WDT } return (CRCINIRES); #else uint8_t j; uint16_t memoryContent; uint16_t crc = CRC16_CCITT_SEED; for(i = 0 ; i < memorySize/2 ; i ++) { // Byte reverse memoryContent = ((*pStartAddress & 0x00FF) << 8) + ((*pStartAddress & 0xFF00) >> 8); for(j = 0 ; j < 16 ; j++) { if((memoryContent ^ crc) >> 15){ crc = (crc << 1) ^ CRC16_CCITT_POLY; }else{ crc <<= 1; } memoryContent <<= 1; } pStartAddress++; } return crc; #endif //__MSP430_HAS_CRC__ }