#include <msp430.h>
#define Num_of_Results 8
volatile unsigned int results[Num_of_Results];
int main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
P6SEL |= 0x01; // Enable A/D channel A0
ADC12CTL0 = ADC12ON+ADC12SHT0_12+ADC12MSC; // Turn on ADC12, set sampling time
ADC12CTL1 = ADC12SHP+ADC12CONSEQ_2; // set multiple sample conversion
// Use sampling timer, set mode
ADC12IE = 0x01; // Enable ADC12IFG.0
ADC12CTL0 |= ADC12ENC; // Enable conversions
ADC12CTL0 |= ADC12SC; // Start conversion
__bis_SR_register(LPM4_bits + GIE); // Enter LPM4, Enable interrupts
}
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
//void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
{
static unsigned char index = 0;
switch(__even_in_range(ADC12IV,34))
{
case 0: break; // Vector 0: No interrupt
case 2: break; // Vector 2: ADC overflow
case 4: break; // Vector 4: ADC timing overflow
case 6: // Vector 6: ADC12IFG0
results[index] = ADC12MEM0; // Move results
index++; // Increment results index, modulo; Set Breakpoint1 here
//if (index == 8)
//{
// index = 0;aaa
//}
case 8: break; // Vector 8: ADC12IFG1
case 10: break; // Vector 10: ADC12IFG2
case 12: break; // Vector 12: ADC12IFG3
case 14: break; // Vector 14: ADC12IFG4
case 16: break; // Vector 16: ADC12IFG5
case 18: break; // Vector 18: ADC12IFG6
case 20: break; // Vector 20: ADC12IFG7
case 22: break; // Vector 22: ADC12IFG8
case 24: break; // Vector 24: ADC12IFG9
case 26: break; // Vector 26: ADC12IFG10
case 28: break; // Vector 28: ADC12IFG11
case 30: break; // Vector 30: ADC12IFG12
case 32: break; // Vector 32: ADC12IFG13
case 34: break; // Vector 34: ADC12IFG14
default: break;
}
}
这是ti提供的AD转换 单通道 连续转换的程序例程 请问 这一转换如何实现连续采样的 执行完中断后怎么回主程序继续执行啊