Other Parts Discussed in Thread: MSP-EXP430FR5994,
Dear TI Team,
Hi,I have a few questions,
Can I replace the 0.22F supercapacitor that comes with the development board? Because my power supply is a DC power supply of about 5V, but the output current is only about 0.2mA, I have to charge for 20 minutes to charge the 0.22F supercapacitor to 2.17V, but the function I use is only the flashing of the LED light, is this the internal 32kHz clock can do it? And I want to do some FFT calculation later, I don't know whether this voltage can be done.
In summary, if I charge the capacitor to 2.17V, can I get the LaunchPad running, and if not, can I replace the supercapacitor on the LaunchPad (0.22F) with some smaller capacitor? How can I solve this problem, look forward to your reply~ Please help me!
Best,
Stone