Part Number: MSP430F149


根据手册,在使用2.0v时,最安全的是使用4Mhz。
但是当电压2.0v时,也可以使用硬件晶振8Mhz。
按目前配置会出现重大隐患吗?还是只要正常启动(起振)就没事了?
还是硬件可以使用8Mhz,软件进行分频到4Mhz就可以了?
还是我理解有问题,请指正一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F149


根据手册,在使用2.0v时,最安全的是使用4Mhz。
但是当电压2.0v时,也可以使用硬件晶振8Mhz。
按目前配置会出现重大隐患吗?还是只要正常启动(起振)就没事了?
还是硬件可以使用8Mhz,软件进行分频到4Mhz就可以了?
还是我理解有问题,请指正一下。
您好

In LF mode, the LFXT1 oscillator requires a watch crystal. TI recommends a 5.1-MΩ resistor from XOUT to VSS when VCC < 2.5 V. In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 4.15 MHz at VCC ≥ 2.2 V. In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 8 MHz at VCC ≥ 2.8 V.
首先根据datasheet显示,在如图测试条件下,您可以使用4Mhz和8Mhz。但是 In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 4.15 MHz at VCC ≥ 2.2 V. 在这个条件官方建议4.15Mhz,表中测试条件VCC=3.3V。不建议您在VCC=2.0V长时间保持8Mhz。In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 8 MHz at VCC ≥ 2.8 V.在这个条件最大可以达到8Mhz。
2.2<vcc<2.5 官方建议您使用4Mhz VCC ≥ 2.8 V 最大可以到达8Mhz。