根据手册,在使用2.0v时,最安全的是使用4Mhz。
但是当电压2.0v时,也可以使用硬件晶振8Mhz。
按目前配置会出现重大隐患吗?还是只要正常启动(起振)就没事了?
还是硬件可以使用8Mhz,软件进行分频到4Mhz就可以了?
还是我理解有问题,请指正一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.


根据手册,在使用2.0v时,最安全的是使用4Mhz。
但是当电压2.0v时,也可以使用硬件晶振8Mhz。
按目前配置会出现重大隐患吗?还是只要正常启动(起振)就没事了?
还是硬件可以使用8Mhz,软件进行分频到4Mhz就可以了?
还是我理解有问题,请指正一下。
您好

In LF mode, the LFXT1 oscillator requires a watch crystal. TI recommends a 5.1-MΩ resistor from XOUT to VSS when VCC < 2.5 V. In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 4.15 MHz at VCC ≥ 2.2 V. In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 8 MHz at VCC ≥ 2.8 V.
首先根据datasheet显示,在如图测试条件下,您可以使用4Mhz和8Mhz。但是 In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 4.15 MHz at VCC ≥ 2.2 V. 在这个条件官方建议4.15Mhz,表中测试条件VCC=3.3V。不建议您在VCC=2.0V长时间保持8Mhz。In XT1 mode, the LFXT1 and XT2 oscillators accept a ceramic resonator or crystal up to 8 MHz at VCC ≥ 2.8 V.在这个条件最大可以达到8Mhz。
2.2<vcc<2.5 官方建议您使用4Mhz VCC ≥ 2.8 V 最大可以到达8Mhz。