1基本要求
1振荡频率≥10KHz
2输出信号电压范围峰-峰值≥2V负载1K欧,500欧50欧
3测量振荡信号参数峰峰值、有效值、频率测量精度要求满足2
的负载下测量误差≤±5%。以外接示波器测试为参考
2发挥部分
指定发挥要求
1 振荡频率 ≥100KHz
2 测量精度提高误差≤±1%以外接示波器测试为参考
3 显示并绘制输入信号波形绘制要求有坐标轴及刻度单位
4 VDD <=3.3V
5 提交设计论文
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.