This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于msp430g2553的简易正弦波发生器设计



 1基本要求

1振荡频率≥10KHz

2输出信号电压范围峰-峰值≥2V负载1K欧,500欧50欧

3测量振荡信号参数峰峰值、有效值、频率测量精度要求满足2

的负载下测量误差≤±5%。以外接示波器测试为参考

2发挥部分

指定发挥要求

1 振荡频率  ≥100KHz

2 测量精度提高误差≤±1%以外接示波器测试为参考

3 显示并绘制输入信号波形绘制要求有坐标轴及刻度单位

4 VDD <=3.3V

5 提交设计论文