This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于MSP430+THM3030优化非接触式M1卡智能门锁方案



在智能门锁系统中,非接触卡读写器的性能格外重要,直接影响到门锁性能、使用寿命以及安全性,关系到酒店的服务质量,因此,选择一款高性能的、高性价比的、信誉品牌高的读写器芯片则至关重要。在NXP、爱特梅尔等芯片厂商长期垄断该市场的情况下,国产芯片厂商北京同方微电子(以下简称同方微电子)凭借在智能卡领域的深厚积累,专门针对门锁行业推出了一款已经有多个成功商用案例的芯片产品THM3030。与目前市场上的同类产品相比,THM3030是一款符合ISO/IEC14443 Type A、M1标准的多协议非接触卡读写器芯片,具有功耗更低、成本更低、读写速度快、易于开发优势,便于开发出更有市场竞争力的产品。

基于MSP430+THM3030优化非接触式M1卡智能门锁方案.docx