請問GPMC支援PSRAM的頻率? 以及工作電壓為1.8V?3.3V?
謝謝~

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于AM261 ZFG和AM261 ZCZ封装,GPMC IO的工作电压=3.3V。测试的闪光灯/PSRAM为3.3V变体。
你能详细说明一下吗?
請問GPMC支援PSRAM的頻率
比如以這家廠商來說:
https://www.issi.com/US/product-asynchronous-sram.shtml#jump5
1.有分布同電壓,因此要選3.3V
www.issi.com/.../66-67WVC2M16EALL.pdf
2.以這顆來說,首先要選 IS66WVC2M16ECLL 支援3.3V,再來是
Operation Frequency up to 104Mhz 
所以請教一下GPMC的CLK頻率規格在哪裡看?支援多少到多少範圍?
謝謝
抱歉耽搁了!!
AM261x中GPMC的最大工作频率为100MHz。
有关更多详细信息,请参阅-AM2612数据表第6.11.5.7节GPMC和 AM261x TRM第6.4.7.2.17节GPMC时钟。
以這顆來說,首先要選 IS66WVC2M16ECLL 支援3.3V,
请注意表13-164中16位非多路模式下GPMC地址线的布线。AM2612 TRM中的GPMC引脚复用选项(及以下注释)。