This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129 ADC1模块中断无法正常进入



        使用TI官方的Tiva™ C Series TM4C129X 开发板,做程序开发时,用ADC1模块配置成sigle-end方式采集时,发现始终无法进入中断,而同样的代码,修改基地址和中断向量表项后,应用于ADC0模块时却可以正常工作,请问这是什么原因,使用ADC1时还需要特殊配置么?

  • 奇怪,不应该呀,是不是ADC1的引脚用作特殊功能了呢?用的是哪个芯片呢?

  • 使用的是Tiva™C系列TM4C129x连接开发套件,具体芯片的型号是:TM4C129NCPDT,大虾你使用过这款芯片的ADC1模块没有?
  • 我的ADC1模块配置代码如下:

    void ADC1IntHandler(void)

    {

           //中断处理代码

           .................................

    }

    void ADC1Init(void)

    {

            SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);

            SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);

            GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1);

            ADCSequenceConfigure(ADC1_BASE, 0, ADC_TRIGGER_PROCESSOR, 0);

            ADCSequenceStepConfigure(ADC1_BASE, 0, 0, ADC_CTL_CH2 | ADC_CTL_IE |
                                                                                                                                             ADC_CTL_END);

            IntEnable(INT_ADC1SS0_BLIIARD);

            ADCIntEnable(ADC1_BASE,0);

            ADCSequenceEnable(ADC1_BASE,0);

    }

    int main()

    {

          //设置系统时钟

         ..........

         //初始化ADC1

         ADC1Init();

         //开总中断

         IntMasterEnable();

        //触发ADC工作

        ADCProcessorTrigger(ADC1_BASE, 0);

        ....................................................

    }

  • TM4C129NCPDT,关键的型号没了。全程应该是TM4C129xNCPDT,你没有给x的值是多少。看了几个版本的数据手册,ADC1应该是PE2脚,你设置的是PE1脚,能读出才怪呢