mspware添加的例程全部报错,两台电脑都这样,系统win10,CCS和mspware全部为最新的,重装CCS和mspware还是报错,但是自己新建的工程可以用,而通过CCS导入的例程,不管什么都会报错,而且全是找不到定义,而程序头文件都有的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
To update CCS Desktop with latest header file support package. Open up CCS and using the drop down menu go to "Help -> Check for Updates".
Make sure to choose "MSP432 Emulators" version "6.2.1.1" (or above) and progress through the installation by clicking "Next". Once CCS has installed and restarted you will have the new CMSIS-Core header files.
As of CCS version 1.4 released on March 15th, the header file support package used in the CCS Cloud IDE supports the latest MSP432 CMSIS-Core header files. There is nothing needed for you to do to update the IDE, instead you need to perform the following steps to download your project and convert it.