This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294 串口转以太网 关于网口设置

Other Parts Discussed in Thread: SW-TM4C, EK-TM4C1294XL, TM4C1294NCPDT

   按照官方的例程 s2e  网线是插在路由器上,动态设置的IP

  请问 如果要通过网线直接链接在电脑上呢?怎么弄 求教大神

  • 这个没搞过,但是电脑也是可以自动获取IP的吧。我记得以前有帖子好像讨论过这个问题来着,你可以翻下以前的帖子。

  • 下载Tivaware  http://software-dl.ti.com/tiva-c/SW-TM4C/latest/index_FDS.html

    安装在本地后,项目文件在如下路径(如果默认路径安装)

    C:\ti\TivaWare_C_Series-2.1.1.71\examples\boards\ek-tm4c1294xl\enet_uip

    项目功能说明如下:

    Ethernet with uIP (enet_uip)
    This example application demonstrates the operation of the Tiva C Series Ethernet controller using
    the uIP TCP/IP Stack. DHCP is used to obtain an Ethernet address. A basic web site is served
    over the Ethernet port. The web site displays a few lines of text, and a counter that increments each
    time the page is sent.
    UART0, connected to the ICDI virtual COM port and running at 115,200, 8-N-1, is used to display
    messages from this application.
    For additional details on uIP, refer to the uIP web page at: http://www.sics.se/adam/uip/

  • 您好,想请问下: TM4C1294NCPDT的uip例程为什么与某些路由器无法通信?

  • 这些应该是路由器的问题,不是所有的路由器都一样的。

  • 你试试在PC上开启DHCP服务,并将本机设为网关地址。