按照官方的例程 s2e 网线是插在路由器上,动态设置的IP
请问 如果要通过网线直接链接在电脑上呢?怎么弄 求教大神
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照官方的例程 s2e 网线是插在路由器上,动态设置的IP
请问 如果要通过网线直接链接在电脑上呢?怎么弄 求教大神
下载Tivaware http://software-dl.ti.com/tiva-c/SW-TM4C/latest/index_FDS.html
安装在本地后,项目文件在如下路径(如果默认路径安装)
C:\ti\TivaWare_C_Series-2.1.1.71\examples\boards\ek-tm4c1294xl\enet_uip
项目功能说明如下:
Ethernet with uIP (enet_uip)
This example application demonstrates the operation of the Tiva C Series Ethernet controller using
the uIP TCP/IP Stack. DHCP is used to obtain an Ethernet address. A basic web site is served
over the Ethernet port. The web site displays a few lines of text, and a counter that increments each
time the page is sent.
UART0, connected to the ICDI virtual COM port and running at 115,200, 8-N-1, is used to display
messages from this application.
For additional details on uIP, refer to the uIP web page at: http://www.sics.se/adam/uip/