如果用DAC8534实现DAC转换该怎么设置?
用SSIConfigSetExpClk()函数只能设置发送数据宽度为4~16,而DAC8534为16位DAC转换芯片,每次发送24为前面八位为控制位,决定从ABCD哪个通道输出。要怎么设置才能实现SSI与DAC8534之间的数据传输呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果用DAC8534实现DAC转换该怎么设置?
用SSIConfigSetExpClk()函数只能设置发送数据宽度为4~16,而DAC8534为16位DAC转换芯片,每次发送24为前面八位为控制位,决定从ABCD哪个通道输出。要怎么设置才能实现SSI与DAC8534之间的数据传输呢?
用哪个库函数进行设置呢?设置完比如说前8位固定0xA0,要发送一个不停变化的16位的数,用变量Num代替。该怎么发送呢?
void SSIDataPut(uint32_t ui32Base, uint32_t ui32Data)
用这个函数发送数据就好了。用num代替ui32Data就好了。注意手册上的这个说明
The upper 32 - N bits of ui32Data are discarded by the hardware, where N is the data width as configured by SSIConfigSetExpClk(). For example, if the interface is configured for 8-bit data width, the upper 24 bits of ui32Data are discarded.
如果发送的是8位数据的话,有24位是无效的。
Num是个16位的啊,怎么能那样发呢?你的意思是不是用SSIDataPut()发送三次,第一次发送前面八位控制位,第二次发送Num的高八位,第三次发送Num的低八位
也就是:
SSIDataPut(SSI0_BASE,0xA0);
SSIDataPut(SSI0_BASE,(0xFF00&Num)>>4);
SSIDataPut(SSI0_BASE,0x00FF&Num);
是这样吗?这样行的通吗?
理论是可以的,具体需要测试。你为什么不把这三个,组合为一个u32的数据呢。
SSIConfigSetExpClk()函数中数据帧长度只能是4~16位,SSIConfigSetExpClk()函数中数据帧长度确定了,SSIDataPut()发送的数据的有效位数就确定了,如果组合成U32怎么发送呢?
我的意思是DAC8534数据输入寄存器的格式是24位的,D23和D22位为地址选择,D21和D20位为输出通道加载位,D19不用管,D18和D17位为信号输出通道选择位,D16位为电源下拉模式选择标志位。后16位为用于DAC转换的数据位。SSIConfigSetExpClk()能发送的数据帧长度范围为4~16,如果要用DAC8534对一个16位的变量实现DAC转换,那么DAC8534数据输入寄存器的前面8位怎么写进去呢?
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
//
while(SSIDataGetNonBlocking(SSI0_BASE, &pui32DataRx[0]))
{
}
//
// Initialize the data to send.
//
pui32DataTx[0] = 's';
pui32DataTx[1] = 'p';
pui32DataTx[2] = 'i';
//
// Display indication that the SSI is transmitting data.
//
UARTprintf("Sent:\n ");
//
// Send 3 bytes of data.
//
for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
{
//
// Display the data that SSI is transferring.
//
UARTprintf("'%c' ", pui32DataTx[ui32Index]);
//
// Send the data using the "blocking" put function. This function
// will wait until there is room in the send FIFO before returning.
// This allows you to assure that all the data you send makes it into
// the send FIFO.
//
SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]);
}
前8位数据左移16位然后和后16位相或不就可以了么。虽然SSIConfigSetExpClk()能发送的数据帧长度范围为4~16,但是
SSIDataPut的参数是u32的。你可以可以单独8位8位的发,一起组合为一个u32的数据需要你测试下,没看数据手册,不知道SSIConfigSetExpClk()能发送的数据帧长度范围为4~16是否就是SSI的FIFO的长度呢?如果是的话,那就不能组合了。