如何实现在TM4C129X开发板的QVGA LCD上显示时间,哪位大神有这方面的代码,参考代码也行?十分感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如何实现在TM4C129X开发板的QVGA LCD上显示时间,哪位大神有这方面的代码,参考代码也行?十分感谢!
/*
Code made with energia-0101E0012
This code is suposed to help clarify anyone with doubts of how to use very basic fuctions of the RTC
in the hibernation peripheral and also the hardware calendar mode. Any sugestions and improvements are always welcome
This example only changes and show hour, minutes and seconds but there's:
psTime->tm_min
psTime->tm_sec
psTime->tm_mon
psTime->tm_mday
psTime->tm_wday
psTime->tm_year
psTime->tm_hour
*/
#include "driverlib/hibernate.c"
void HibernateHandler(void)
{
//Use this to reset interrupt flag
uint32_t ui32Status = HibernateIntStatus(1);
HibernateIntClear(ui32Status);
//Place here code to execute every second, ex: LCD or 7 segment display
//Altough it should be as fastest as possible
//To keep the interrupt hapening every second you need this
HibernateRTCMatchSet(0,HibernateRTCGet()+1);
}
/*It's need a struct pointer of the type "tm" so i use new to do that. This type of struct is defined in the driverlib/hibernation
you could also create it like this: tm temp; and then use &temp and temp.values in the fuctions
*/
tm *temp = new tm;
void setup()
{
Serial.begin(9600);
// put your setup code here, to run once:
//Enable Hibernate peripheral. I'm using Energia so i use F_CPU for geting the clock frequency
HibernateEnableExpClk(F_CPU);
HibernateRTCEnable();
//We set a interrupt for the RTC after second. You can change the value
HibernateRTCMatchSet(0,HibernateRTCGet()+1);
HibernateIntRegister(HibernateHandler);
HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0);
//Set up calender mode. HibernateCounterMode() is always needed but can be set to 12hr mode
HibernateCounterMode(HIBERNATE_COUNTER_24HR);
HibernateCalendarSet(temp); //<-- the struct declared
//We change the hour, minutes and seconds
temp->tm_hour= 23;
temp->tm_min=59;
temp->tm_sec = 50;
//This fuction below is what actualy updates the values inside the peripheral.
//if you don't use it, the value changes above won't do anytigh
HibernateCalendarSet(temp);
}
void loop()
{
//This is to take the "live" values that the RTC keeps updating into our struct
HibernateCalendarGet(temp);
Serial.print(temp->tm_hour);
Serial.print(':');
Serial.print(temp->tm_min);
Serial.print(':');
Serial.println(temp->tm_sec);
delay(1000);
}
网上找到的。没验证过,使用的是RTC的功能,自己对照的库函数的数据手册看吧。
是有RTC模式的,但是没有用过,是否可以像RTC时钟芯片那样,自动计算时间日期呢,你需要具体研究下。