This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tm4c129x时钟显示



如何实现在TM4C129X开发板的QVGA LCD上显示时间,哪位大神有这方面的代码,参考代码也行?十分感谢!

  • /*
    
      Code made with energia-0101E0012
    
      This code is suposed to help clarify anyone with doubts of how to use very basic fuctions of the RTC
      in the hibernation peripheral and also the hardware calendar mode. Any sugestions and improvements are always welcome
      
      This example only changes and show hour, minutes and seconds but there's:
        psTime->tm_min
        psTime->tm_sec 
        psTime->tm_mon 
        psTime->tm_mday 
        psTime->tm_wday 
        psTime->tm_year
        psTime->tm_hour
    
    */
    #include "driverlib/hibernate.c"
    
    
    void HibernateHandler(void)
    {
      //Use this to reset interrupt flag
      uint32_t ui32Status = HibernateIntStatus(1);
      HibernateIntClear(ui32Status);
      
      //Place here code to execute every second, ex: LCD or 7 segment display
      //Altough it should be as fastest as possible
      
      
      //To keep the interrupt hapening every second you need this
      HibernateRTCMatchSet(0,HibernateRTCGet()+1);  
    }
    
    /*It's need a struct pointer of the type "tm" so i use new to do that. This type of struct is defined in the driverlib/hibernation
      you could also create it like this: tm temp; and then use &temp and temp.values in the fuctions                              
    */
    tm *temp = new tm;
    
    
    
    void setup()
    {
      Serial.begin(9600);
      // put your setup code here, to run once:
      
      //Enable Hibernate peripheral. I'm using Energia so i use F_CPU for geting the clock frequency
      HibernateEnableExpClk(F_CPU);
      HibernateRTCEnable();
      
      //We set a interrupt for the RTC after second. You can change the value
      HibernateRTCMatchSet(0,HibernateRTCGet()+1);
      HibernateIntRegister(HibernateHandler);
      HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0);
      
      //Set up calender mode. HibernateCounterMode() is always needed but can be set to 12hr mode
      HibernateCounterMode(HIBERNATE_COUNTER_24HR);
      HibernateCalendarSet(temp); //<-- the struct declared
      
      //We change the hour, minutes and seconds
      temp->tm_hour= 23;
      temp->tm_min=59;
      temp->tm_sec = 50;
      //This fuction below is what actualy updates the values inside the peripheral. 
      //if you don't use it, the value changes above won't do anytigh
      HibernateCalendarSet(temp);
      
    }
    
    void loop()
    {
      //This is to take the "live" values that the RTC keeps updating into our struct
      HibernateCalendarGet(temp);
      Serial.print(temp->tm_hour);
       Serial.print(':'); 
       Serial.print(temp->tm_min);
      Serial.print(':'); 
      Serial.println(temp->tm_sec);
      delay(1000);
    }
    

    网上找到的。没验证过,使用的是RTC的功能,自己对照的库函数的数据手册看吧。

  • TM4C129X有内置的RTC吗?可以显示实时时间吗

  • 是有RTC模式的,但是没有用过,是否可以像RTC时钟芯片那样,自动计算时间日期呢,你需要具体研究下。

  • 他有RTC的例程吗?

  • 看我二楼的程序,官方没提供例程。