This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在想要一个1s的定时器中断,在cc1310中并且在RTOS系统中怎么产生
HI,请参考:
// Convenience macro to make the code more readable // Set Clock.tickPeriod in the .cfg file #define Clock_convertSecondsToTicks(seconds) \ (((seconds) * 1000000) / (Clock_tickPeriod)) // Solution 1 // ---------- // Reserve memory for the clock object Clock_Struct clock; uint32_t timeoutTicks = Clock_convertSecondsToTicks(30); // Create a one-shot timer Clock_construct(&clock, &Serial_TimerCallback, timeoutTicks, NULL); // Start the timer Clock_start(Clock_handle(&clock)); // Solution 2 // ---------- uint32_t timeoutTicks = Clock_convertSecondsToTicks(30); // Create a one-shot timer somewhere on the heap Clock_Handle clock = Clock_create(&Serial_TimerCallback, timeoutTicks, NULL, NULL); // Start the timer Clock_start(clock); // Solution 3 // ---------- // Create a static clock object in the .cfg file // The init code is automatically generated by xdctools var clock0Params = new Clock.Params(); clock0Params.instance.name = "clock"; Program.global.clock = Clock.create("&Serial_TimerCallback", 30, clock0Params); // Start the clock somewhere in your program extern const Clock_Handle clock; Clock_start(clock);