This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM关于I2C的固件库编程,关于6050陀螺仪



因为初次接触TM4c的I2C的固件库操作,不想用GPIO口模拟I2C操作,但是在使用的时候出现了一点问题,陀螺仪6050的数据完全读不出来,我6050只接了4根线,分别是VCC,GND,SCL,SDA,这里有部分代码

uchar data[8] = {0};
//设置时钟,为外部晶振,一分频,16MHZ
SysCtlClockSet(SYSCTL_SYSDIV_1|SYSCTL_USE_OSC|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
InitConsole();
//使用的是I2C0,所以所用的SCL和SDA是用PB2和B3
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);

GPIOPinTypeI2C(GPIO_PORTB_BASE,GPIO_PIN_3);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE,GPIO_PIN_2);
//false为100kbit/s,true为400kbit/s
I2CMasterInitExpClk(I2C0_BASE,SysCtlClockGet(),false);
//设置从机地址 false 向从机发送信号,true接收从机的信号
UARTprintf("the\n");
//使能从机模块,基地址为where_i2c
I2CSlaveEnable(where_i2c);
I2CMasterSlaveAddrSet(I2C0_BASE,where_i2c,true);

UARTprintf("the\n");
//空接收数据,确保接收到的第一个数据不会是空数据
I2CMasterControl(I2C0_BASE,I2C_MASTER_CMD_SINGLE_RECEIVE);
//等待从主机来的接收请求
/*
while(!(I2CSlaveStatus(I2C0_BASE)&I2C_SLAVE_ACT_TREQ))
{
}
*/
while(1)
{
// for(;i < 8;i++)
{
//读取一个数据,到数据寄存器中
// I2CSlaveDataPut(I2C0_BASE,data[i]);
//告诉主机读取数据了
I2CMasterControl(I2C0_BASE,I2C_MASTER_CMD_SINGLE_RECEIVE);
//等待数据发送完成
// while(!(I2CSlaveStatus(I2C0_BASE)&I2C_SLAVE_ACT_TREQ))
// {

// }
data[0] = I2CSlaveDataGet(I2C0_BASE);

UARTprintf("data[0] = %c\n",data[0]);

希望能得到解答,UART只是用来调试用的


}
SysCtlDelay(SysCtlClockGet()/3);
UARTprintf("-------------------------\n");
// i= 0;
}

  • 关于mpu6050的驱动,TI是提供了第三方的库的

    //*****************************************************************************
    //
    // mpu6050.c - Driver for the MPU6050 accelerometer and gyroscope.
    //
    // Copyright (c) 2013-2017 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.1.4.178 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #include <stdint.h>
    #include "sensorlib/hw_mpu6050.h"
    #include "sensorlib/i2cm_drv.h"
    #include "sensorlib/mpu6050.h"
    
    //*****************************************************************************
    //
    //! \addtogroup mpu6050_api
    //! @{
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // The states of the MPU6050 state machine.
    //
    //*****************************************************************************
    #define MPU6050_STATE_IDLE      0           // State machine is idle
    #define MPU6050_STATE_INIT_RES  1           // Waiting for initialization
    #define MPU6050_STATE_INIT_WAIT 2           // Waiting for reset to complete
    #define MPU6050_STATE_READ      3           // Waiting for read
    #define MPU6050_STATE_WRITE     4           // Waiting for write
    #define MPU6050_STATE_RMW       5           // Waiting for read-modify-write
    
    //*****************************************************************************
    //
    // The factors used to convert the acceleration readings from the MPU6050 into
    // floating point values in meters per second squared.
    //
    // Values are obtained by taking the g conversion factors from the data sheet
    // and multiplying by 9.81 (1 g = 9.81 m/s^2).
    //
    //*****************************************************************************
    static const float g_fMPU6050AccelFactors[] =
    {
        0.00059875,                              // Range = +/- 2 g (16384 lsb/g)
        0.00119751,                              // Range = +/- 4 g (8192 lsb/g)
        0.00239502,                              // Range = +/- 8 g (4096 lsb/g)
        0.00479004                               // Range = +/- 16 g (2048 lsb/g)
    };
    
    //*****************************************************************************
    //
    // The factors used to convert the acceleration readings from the MPU6050 into
    // floating point values in radians per second.
    //
    // Values are obtained by taking the degree per second conversion factors
    // from the data sheet and then converting to radians per sec (1 degree =
    // 0.0174532925 radians).
    //
    //*****************************************************************************
    static const float g_fMPU6050GyroFactors[] =
    {
        1.3323124e-4f,   // Range = +/- 250 dps  (131.0 LSBs/DPS)
        2.6646248e-4f,   // Range = +/- 500 dps  (65.5 LSBs/DPS)
        5.3211258e-4f,   // Range = +/- 1000 dps (32.8 LSBs/DPS)
        0.0010642252f    // Range = +/- 2000 dps (16.4 LSBs/DPS)
    };
    //*****************************************************************************
    //
    // The callback function that is called when I2C transations to/from the
    // MPU6050 have completed.
    //
    //*****************************************************************************
    static void
    MPU6050Callback(void *pvCallbackData, uint_fast8_t ui8Status)
    {
        tMPU6050 *psInst;
    
        //
        // Convert the instance data into a pointer to a tMPU6050 structure.
        //
        psInst = pvCallbackData;
    
        //
        // If the I2C master driver encountered a failure, force the state machine
        // to the idle state (which will also result in a callback to propagate the
        // error).  Except in the case that we are in the reset wait state and the
        // error is an address NACK.  This error is handled by the reset wait
        // state.
        //
        if((ui8Status != I2CM_STATUS_SUCCESS) &&
            !((ui8Status == I2CM_STATUS_ADDR_NACK) &&
                (psInst->ui8State == MPU6050_STATE_INIT_WAIT)))
        {
            psInst->ui8State = MPU6050_STATE_IDLE;
        }
    
        //
        // Determine the current state of the MPU6050 state machine.
        //
        switch(psInst->ui8State)
        {
            //
            // All states that trivially transition to IDLE, and all unknown
            // states.
            //
            case MPU6050_STATE_READ:
            default:
            {
                //
                // The state machine is now idle.
                //
                psInst->ui8State = MPU6050_STATE_IDLE;
    
                //
                // Done.
                //
                break;
            }
    
            //
            // MPU6050 Device reset was issued
            //
            case MPU6050_STATE_INIT_RES:
            {
                //
                // Issue a read of the status register to confirm reset is done.
                //
                psInst->uCommand.pui8Buffer[0] = MPU6050_O_PWR_MGMT_1;
                I2CMRead(psInst->psI2CInst, psInst->ui8Addr,
                         psInst->uCommand.pui8Buffer, 1, psInst->pui8Data, 1,
                         MPU6050Callback, psInst);
    
                psInst->ui8State = MPU6050_STATE_INIT_WAIT;
                break;
            }
    
            //
            // Status register was read, check if reset is done before proceeding.
            //
            case MPU6050_STATE_INIT_WAIT:
            {
                //
                // Check the value read back from status to determine if device
                // is still in reset or if it is ready.  Reset state for this
                // register is 0x40, which has sleep bit set.  Device may also
                // respond with an address NACK during very early stages of the its
                // internal reset. Keep polling until we verify device is ready.
                //
                //
                if((psInst->pui8Data[0] != MPU6050_PWR_MGMT_1_SLEEP) ||
                    (ui8Status == I2CM_STATUS_ADDR_NACK))
                {
                    //
                    // Device still in reset so begin polling this register.
                    //
                    psInst->uCommand.pui8Buffer[0] = MPU6050_O_PWR_MGMT_1;
                    I2CMRead(psInst->psI2CInst, psInst->ui8Addr,
                             psInst->uCommand.pui8Buffer, 1, psInst->pui8Data, 1,
                             MPU6050Callback, psInst);
    
                    //
                    // Intentionally stay in this state to create polling effect.
                    //
                }
                else
                {
                    //
                    // Device is out of reset, move to the idle state.
                    //
                    psInst->ui8State = MPU6050_STATE_IDLE;
                }
                break;
            }
    
            //
            // A write just completed
            //
            case MPU6050_STATE_WRITE:
            {
                //
                // Set the accelerometer and gyroscope ranges to the new values.
                // If the register was not modified, the values will be the same so
                // this has no effect.
                //
                psInst->ui8AccelAfsSel = psInst->ui8NewAccelAfsSel;
                psInst->ui8GyroFsSel = psInst->ui8NewGyroFsSel;
    
                //
                // The state machine is now idle.
                //
                psInst->ui8State = MPU6050_STATE_IDLE;
    
                //
                // Done.
                //
                break;
            }
    
            //
            // A read-modify-write just completed
            //
            case MPU6050_STATE_RMW:
            {
                //
                // See if the PWR_MGMT_1 register was just modified.
                //
                if(psInst->uCommand.sReadModifyWriteState.pui8Buffer[0] ==
                   MPU6050_O_PWR_MGMT_1)
                {
                    //
                    // See if a soft reset has been issued.
                    //
                    if(psInst->uCommand.sReadModifyWriteState.pui8Buffer[1] &
                       MPU6050_PWR_MGMT_1_DEVICE_RESET)
                    {
                        //
                        // Default range setting is +/- 2 g
                        //
                        psInst->ui8AccelAfsSel = 0;
                        psInst->ui8NewAccelAfsSel = 0;
    
                        //
                        // Default range setting is +/- 250 degrees/s
                        //
                        psInst->ui8GyroFsSel = 0;
                        psInst->ui8NewGyroFsSel = 0;
                    }
                }
    
                //
                // See if the GYRO_CONFIG register was just modified.
                //
                if(psInst->uCommand.sReadModifyWriteState.pui8Buffer[0] ==
                   MPU6050_O_GYRO_CONFIG)
                {
                    //
                    // Extract the FS_SEL from the GYRO_CONFIG register value.
                    //
                    psInst->ui8GyroFsSel =
                        ((psInst->uCommand.sReadModifyWriteState.pui8Buffer[1] &
                          MPU6050_GYRO_CONFIG_FS_SEL_M) >>
                         MPU6050_GYRO_CONFIG_FS_SEL_S);
                }
    
                //
                // See if the ACCEL_CONFIG register was just modified.
                //
                if(psInst->uCommand.sReadModifyWriteState.pui8Buffer[0] ==
                   MPU6050_O_ACCEL_CONFIG)
                {
                    //
                    // Extract the FS_SEL from the ACCEL_CONFIG register value.
                    //
                    psInst->ui8AccelAfsSel =
                        ((psInst->uCommand.sReadModifyWriteState.pui8Buffer[1] &
                          MPU6050_ACCEL_CONFIG_AFS_SEL_M) >>
                         MPU6050_ACCEL_CONFIG_AFS_SEL_S);
                }
    
                //
                // The state machine is now idle.
                //
                psInst->ui8State = MPU6050_STATE_IDLE;
    
                //
                // Done.
                //
                break;
            }
        }
    
        //
        // See if the state machine is now idle and there is a callback function.
        //
        if((psInst->ui8State == MPU6050_STATE_IDLE) && psInst->pfnCallback)
        {
            //
            // Call the application-supplied callback function.
            //
            psInst->pfnCallback(psInst->pvCallbackData, ui8Status);
        }
    }
    
    //*****************************************************************************
    //
    //! Initializes the MPU6050 driver.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param psI2CInst is a pointer to the I2C master driver instance data.
    //! \param ui8I2CAddr is the I2C address of the MPU6050 device.
    //! \param pfnCallback is the function to be called when the initialization has
    //! completed (can be \b NULL if a callback is not required).
    //! \param pvCallbackData is a pointer that is passed to the callback function.
    //!
    //! This function initializes the MPU6050 driver, preparing it for operation.
    //!
    //! \return Returns 1 if the MPU6050 driver was successfully initialized and 0
    //! if it was not.
    //
    //*****************************************************************************
    uint_fast8_t
    MPU6050Init(tMPU6050 *psInst, tI2CMInstance *psI2CInst,
                uint_fast8_t ui8I2CAddr, tSensorCallback *pfnCallback,
                void *pvCallbackData)
    {
        //
        // Initialize the MPU6050 instance structure.
        //
        psInst->psI2CInst = psI2CInst;
        psInst->ui8Addr = ui8I2CAddr;
    
        //
        // Save the callback information.
        //
        psInst->pfnCallback = pfnCallback;
        psInst->pvCallbackData = pvCallbackData;
    
        //
        // Default range setting is +/- 2 g
        //
        psInst->ui8AccelAfsSel = (MPU6050_ACCEL_CONFIG_AFS_SEL_2G >>
                                  MPU6050_ACCEL_CONFIG_AFS_SEL_S);
        psInst->ui8NewAccelAfsSel = (MPU6050_ACCEL_CONFIG_AFS_SEL_2G >>
                                     MPU6050_ACCEL_CONFIG_AFS_SEL_S);
    
        //
        // Default range setting is +/- 250 degrees/s
        //
        psInst->ui8GyroFsSel = (MPU6050_GYRO_CONFIG_FS_SEL_250 >>
                                MPU6050_GYRO_CONFIG_FS_SEL_S);
        psInst->ui8NewGyroFsSel = (MPU6050_GYRO_CONFIG_FS_SEL_250 >>
                                   MPU6050_GYRO_CONFIG_FS_SEL_S);
    
        //
        // Set the state to show we are initiating a reset.
        //
        psInst->ui8State = MPU6050_STATE_INIT_RES;
    
        //
        // Load the buffer with command to perform device reset
        //
        psInst->uCommand.pui8Buffer[0] = MPU6050_O_PWR_MGMT_1;
        psInst->uCommand.pui8Buffer[1] = MPU6050_PWR_MGMT_1_DEVICE_RESET;
        if(I2CMWrite(psInst->psI2CInst, psInst->ui8Addr,
                     psInst->uCommand.pui8Buffer, 2, MPU6050Callback, psInst) == 0)
        {
            psInst->ui8State = MPU6050_STATE_IDLE;
            return(0);
        }
    
        //
        // Success
        //
        return(1);
    }
    
    //*****************************************************************************
    //
    //! Reads data from MPU6050 registers.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param ui8Reg is the first register to read.
    //! \param pui8Data is a pointer to the location to store the data that is
    //! read.
    //! \param ui16Count is the number of data bytes to read.
    //! \param pfnCallback is the function to be called when the data has been read
    //! (can be \b NULL if a callback is not required).
    //! \param pvCallbackData is a pointer that is passed to the callback function.
    //!
    //! This function reads a sequence of data values from consecutive registers in
    //! the MPU6050.
    //!
    //! \return Returns 1 if the write was successfully started and 0 if it was
    //! not.
    //
    //*****************************************************************************
    uint_fast8_t
    MPU6050Read(tMPU6050 *psInst, uint_fast8_t ui8Reg, uint8_t *pui8Data,
                uint_fast16_t ui16Count, tSensorCallback *pfnCallback,
                void *pvCallbackData)
    {
        //
        // Return a failure if the MPU6050 driver is not idle (in other words,
        // there is already an outstanding request to the MPU6050).
        //
        if(psInst->ui8State != MPU6050_STATE_IDLE)
        {
            return(0);
        }
    
        //
        // Save the callback information.
        //
        psInst->pfnCallback = pfnCallback;
        psInst->pvCallbackData = pvCallbackData;
    
        //
        // Move the state machine to the wait for read state.
        //
        psInst->ui8State = MPU6050_STATE_READ;
    
        //
        // Read the requested registers from the MPU6050.
        //
        psInst->uCommand.pui8Buffer[0] = ui8Reg;
        if(I2CMRead(psInst->psI2CInst, psInst->ui8Addr,
                    psInst->uCommand.pui8Buffer, 1, pui8Data, ui16Count,
                    MPU6050Callback, psInst) == 0)
        {
            //
            // The I2C write failed, so move to the idle state and return a
            // failure.
            //
            psInst->ui8State = MPU6050_STATE_IDLE;
            return(0);
        }
    
        //
        // Success.
        //
        return(1);
    }
    
    //*****************************************************************************
    //
    //! Writes data to MPU6050 registers.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param ui8Reg is the first register to write.
    //! \param pui8Data is a pointer to the data to write.
    //! \param ui16Count is the number of data bytes to write.
    //! \param pfnCallback is the function to be called when the data has been
    //! written (can be \b NULL if a callback is not required).
    //! \param pvCallbackData is a pointer that is passed to the callback function.
    //!
    //! This function writes a sequence of data values to consecutive registers in
    //! the MPU6050.  The first byte of the \e pui8Data buffer contains the value
    //! to be written into the \e ui8Reg register, the second value contains the
    //! data to be written into the next register, and so on.
    //!
    //! \return Returns 1 if the write was successfully started and 0 if it was
    //! not.
    //
    //*****************************************************************************
    uint_fast8_t
    MPU6050Write(tMPU6050 *psInst, uint_fast8_t ui8Reg, const uint8_t *pui8Data,
                 uint_fast16_t ui16Count, tSensorCallback *pfnCallback,
                 void *pvCallbackData)
    {
        //
        // Return a failure if the MPU6050 driver is not idle (in other words,
        // there is already an outstanding request to the MPU6050).
        //
        if(psInst->ui8State != MPU6050_STATE_IDLE)
        {
            return(0);
        }
    
        //
        // Save the callback information.
        //
        psInst->pfnCallback = pfnCallback;
        psInst->pvCallbackData = pvCallbackData;
    
        //
        // See if the PWR_MGMT_1 register is being written.
        //
        if((ui8Reg <= MPU6050_O_PWR_MGMT_1) &&
           ((ui8Reg + ui16Count) > MPU6050_O_PWR_MGMT_1))
        {
            //
            // See if a soft reset is being requested.
            //
            if(pui8Data[ui8Reg - MPU6050_O_PWR_MGMT_1] &
               MPU6050_PWR_MGMT_1_DEVICE_RESET)
            {
                //
                // Default range setting is +/- 2 g.
                //
                psInst->ui8NewAccelAfsSel = 0;
    
                //
                // Default range setting is +/- 250 degrees/s.
                //
                psInst->ui8NewGyroFsSel = 0;
            }
        }
    
        //
        // See if the GYRO_CONFIG register is being written.
        //
        if((ui8Reg <= MPU6050_O_GYRO_CONFIG) &&
           ((ui8Reg + ui16Count) > MPU6050_O_GYRO_CONFIG))
        {
            //
            // Extract the FS_SEL from the GYRO_CONFIG register value.
            //
            psInst->ui8NewGyroFsSel = ((pui8Data[ui8Reg - MPU6050_O_GYRO_CONFIG] &
                                        MPU6050_GYRO_CONFIG_FS_SEL_M) >>
                                       MPU6050_GYRO_CONFIG_FS_SEL_S);
        }
    
        //
        // See if the ACCEL_CONFIG register is being written.
        //
        if((ui8Reg <= MPU6050_O_ACCEL_CONFIG) &&
           ((ui8Reg + ui16Count) > MPU6050_O_ACCEL_CONFIG))
        {
            //
            // Extract the AFS_SEL from the ACCEL_CONFIG register value.
            //
            psInst->ui8NewAccelAfsSel =
                ((pui8Data[ui8Reg - MPU6050_O_ACCEL_CONFIG] &
                  MPU6050_ACCEL_CONFIG_AFS_SEL_M) >>
                 MPU6050_ACCEL_CONFIG_AFS_SEL_S);
        }
    
        //
        // Move the state machine to the wait for write state.
        //
        psInst->ui8State = MPU6050_STATE_WRITE;
    
        //
        // Write the requested registers to the MPU6050.
        //
        if(I2CMWrite8(&(psInst->uCommand.sWriteState), psInst->psI2CInst,
                      psInst->ui8Addr, ui8Reg, pui8Data, ui16Count,
                      MPU6050Callback, psInst) == 0)
        {
            //
            // The I2C write failed, so move to the idle state and return a
            // failure.
            //
            psInst->ui8State = MPU6050_STATE_IDLE;
            return(0);
        }
    
        //
        // Success.
        //
        return(1);
    }
    
    //*****************************************************************************
    //
    //! Performs a read-modify-write of a MPU6050 register.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param ui8Reg is the register to modify.
    //! \param ui8Mask is the bit mask that is ANDed with the current register
    //! value.
    //! \param ui8Value is the bit mask that is ORed with the result of the AND
    //! operation.
    //! \param pfnCallback is the function to be called when the data has been
    //! changed (can be \b NULL if a callback is not required).
    //! \param pvCallbackData is a pointer that is passed to the callback function.
    //!
    //! This function changes the value of a register in the MPU6050 via a
    //! read-modify-write operation, allowing one of the fields to be changed
    //! without disturbing the other fields.  The \e ui8Reg register is read, ANDed
    //! with \e ui8Mask, ORed with \e ui8Value, and then written back to the
    //! MPU6050.
    //!
    //! \return Returns 1 if the read-modify-write was successfully started and 0
    //! if it was not.
    //
    //*****************************************************************************
    uint_fast8_t
    MPU6050ReadModifyWrite(tMPU6050 *psInst, uint_fast8_t ui8Reg,
                           uint_fast8_t ui8Mask, uint_fast8_t ui8Value,
                           tSensorCallback *pfnCallback, void *pvCallbackData)
    {
        //
        // Return a failure if the MPU6050 driver is not idle (in other words,
        // there is already an outstanding request to the MPU6050).
        //
        if(psInst->ui8State != MPU6050_STATE_IDLE)
        {
            return(0);
        }
    
        //
        // Save the callback information.
        //
        psInst->pfnCallback = pfnCallback;
        psInst->pvCallbackData = pvCallbackData;
    
        //
        // Move the state machine to the wait for read-modify-write state.
        //
        psInst->ui8State = MPU6050_STATE_RMW;
    
        //
        // Submit the read-modify-write request to the MPU6050.
        //
        if(I2CMReadModifyWrite8(&(psInst->uCommand.sReadModifyWriteState),
                                psInst->psI2CInst, psInst->ui8Addr, ui8Reg,
                                ui8Mask, ui8Value, MPU6050Callback, psInst) == 0)
        {
            //
            // The I2C read-modify-write failed, so move to the idle state and
            // return a failure.
            //
            psInst->ui8State = MPU6050_STATE_IDLE;
            return(0);
        }
    
        //
        // Success.
        //
        return(1);
    }
    
    //*****************************************************************************
    //
    //! Reads the accelerometer and gyroscope data from the MPU6050.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param pfnCallback is the function to be called when the data has been read
    //! (can be \b NULL if a callback is not required).
    //! \param pvCallbackData is a pointer that is passed to the callback function.
    //!
    //! This function initiates a read of the MPU6050 data registers.  When the
    //! read has completed (as indicated by calling the callback function), the new
    //! readings can be obtained via:
    //!
    //! - MPU6050DataAccelGetRaw()
    //! - MPU6050DataAccelGetFloat()
    //! - MPU6050DataGyroGetRaw()
    //! - MPU6050DataGyroGetFloat()
    //!
    //! \return Returns 1 if the read was successfully started and 0 if it was not.
    //
    //*****************************************************************************
    uint_fast8_t
    MPU6050DataRead(tMPU6050 *psInst, tSensorCallback *pfnCallback,
                    void *pvCallbackData)
    {
        //
        // Return a failure if the MPU6050 driver is not idle (in other words,
        // there is already an outstanding request to the MPU6050).
        //
        if(psInst->ui8State != MPU6050_STATE_IDLE)
        {
            return(0);
        }
    
        //
        // Save the callback information.
        //
        psInst->pfnCallback = pfnCallback;
        psInst->pvCallbackData = pvCallbackData;
    
        //
        // Move the state machine to the wait for data read state.
        //
        psInst->ui8State = MPU6050_STATE_READ;
    
        //
        // Read the data registers from the MPU6050.
        //
        psInst->pui8Data[0] = MPU6050_O_ACCEL_XOUT_H;
        if(I2CMRead(psInst->psI2CInst, psInst->ui8Addr, psInst->pui8Data, 1,
                    psInst->pui8Data, 14, MPU6050Callback, psInst) == 0)
        {
            //
            // The I2C read failed, so move to the idle state and return a failure.
            //
            psInst->ui8State = MPU6050_STATE_IDLE;
            return(0);
        }
    
        //
        // Success.
        //
        return(1);
    }
    
    //*****************************************************************************
    //
    //! Gets the raw accelerometer data from the most recent data read.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param pui16AccelX is a pointer to the value into which the raw X-axis
    //! accelerometer data is stored.
    //! \param pui16AccelY is a pointer to the value into which the raw Y-axis
    //! accelerometer data is stored.
    //! \param pui16AccelZ is a pointer to the value into which the raw Z-axis
    //! accelerometer data is stored.
    //!
    //! This function returns the raw accelerometer data from the most recent data
    //! read.  The data is not manipulated in any way by the driver.  If any of the
    //! output data pointers are \b NULL, the corresponding data is not provided.
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    MPU6050DataAccelGetRaw(tMPU6050 *psInst, uint_fast16_t *pui16AccelX,
                           uint_fast16_t *pui16AccelY, uint_fast16_t *pui16AccelZ)
    {
        //
        // Return the raw accelerometer values.
        //
        if(pui16AccelX)
        {
            *pui16AccelX = (psInst->pui8Data[0] << 8) | psInst->pui8Data[1];
        }
        if(pui16AccelY)
        {
            *pui16AccelY = (psInst->pui8Data[2] << 8) | psInst->pui8Data[3];
        }
        if(pui16AccelZ)
        {
            *pui16AccelZ = (psInst->pui8Data[4] << 8) | psInst->pui8Data[5];
        }
    }
    
    //*****************************************************************************
    //
    //! Gets the accelerometer data from the most recent data read.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param pfAccelX is a pointer to the value into which the X-axis
    //! accelerometer data is stored.
    //! \param pfAccelY is a pointer to the value into which the Y-axis
    //! accelerometer data is stored.
    //! \param pfAccelZ is a pointer to the value into which the Z-axis
    //! accelerometer data is stored.
    //!
    //! This function returns the accelerometer data from the most recent data
    //! read, converted into meters per second squared (m/s^2).  If any of the
    //! output data pointers are \b NULL, the corresponding data is not provided.
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    MPU6050DataAccelGetFloat(tMPU6050 *psInst, float *pfAccelX, float *pfAccelY,
                             float *pfAccelZ)
    {
        float fFactor;
    
        //
        // Get the acceleration conversion factor for the current data format.
        //
        fFactor = g_fMPU6050AccelFactors[psInst->ui8AccelAfsSel];
    
        //
        // Convert the Accelerometer values into floating-point gravity values.
        //
        if(pfAccelX)
        {
            *pfAccelX = (float)((int16_t)((psInst->pui8Data[0] << 8) |
                                          psInst->pui8Data[1]) * fFactor);
        }
        if(pfAccelY)
        {
            *pfAccelY = (float)((int16_t)((psInst->pui8Data[2] << 8) |
                                          psInst->pui8Data[3]) * fFactor);
        }
        if(pfAccelZ)
        {
            *pfAccelZ = (float)((int16_t)((psInst->pui8Data[4] << 8) |
                                          psInst->pui8Data[5]) * fFactor);
        }
    }
    //*****************************************************************************
    //
    //! Gets the raw gyroscope data from the most recent data read.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param pui16GyroX is a pointer to the value into which the raw X-axis
    //! gyroscope data is stored.
    //! \param pui16GyroY is a pointer to the value into which the raw Y-axis
    //! gyroscope data is stored.
    //! \param pui16GyroZ is a pointer to the value into which the raw Z-axis
    //! gyroscope data is stored.
    //!
    //! This function returns the raw gyroscope data from the most recent data
    //! read.  The data is not manipulated in any way by the driver.  If any of the
    //! output data pointers are \b NULL, the corresponding data is not provided.
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    MPU6050DataGyroGetRaw(tMPU6050 *psInst, uint_fast16_t *pui16GyroX,
                          uint_fast16_t *pui16GyroY, uint_fast16_t *pui16GyroZ)
    {
        //
        // Return the raw gyroscope values.
        //
        if(pui16GyroX)
        {
            *pui16GyroX = (psInst->pui8Data[8] << 8) | psInst->pui8Data[9];
        }
        if(pui16GyroY)
        {
            *pui16GyroY = (psInst->pui8Data[10] << 8) | psInst->pui8Data[11];
        }
        if(pui16GyroZ)
        {
            *pui16GyroZ = (psInst->pui8Data[12] << 8) | psInst->pui8Data[13];
        }
    }
    
    //*****************************************************************************
    //
    //! Gets the gyroscope data from the most recent data read.
    //!
    //! \param psInst is a pointer to the MPU6050 instance data.
    //! \param pfGyroX is a pointer to the value into which the X-axis
    //! gyroscope data is stored.
    //! \param pfGyroY is a pointer to the value into which the Y-axis
    //! gyroscope data is stored.
    //! \param pfGyroZ is a pointer to the value into which the Z-axis
    //! gyroscope data is stored.
    //!
    //! This function returns the gyroscope data from the most recent data read,
    //! converted into radians per second.  If any of the output data pointers are
    //! \b NULL, the corresponding data is not provided.
    //!
    //! \return None.
    //
    //*****************************************************************************
    void
    MPU6050DataGyroGetFloat(tMPU6050 *psInst, float *pfGyroX, float *pfGyroY,
                            float *pfGyroZ)
    {
        float fFactor;
    
        //
        // Get the conversion factor for the current data format.
        //
        fFactor = g_fMPU6050GyroFactors[psInst->ui8GyroFsSel];
    
        //
        // Convert the gyroscope values into rad/sec
        //
        if(pfGyroX)
        {
            *pfGyroX = ((float)(int16_t)((psInst->pui8Data[8] << 8) |
                                         psInst->pui8Data[9]) * fFactor);
        }
        if(pfGyroY)
        {
            *pfGyroY = ((float)(int16_t)((psInst->pui8Data[10] << 8) |
                                         psInst->pui8Data[11]) * fFactor);
        }
        if(pfGyroZ)
        {
            *pfGyroZ = ((float)(int16_t)((psInst->pui8Data[12] << 8) |
                                         psInst->pui8Data[13]) * fFactor);
        }
    }
    
    //*****************************************************************************
    //
    // Close the Doxygen group.
    //! @}
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // mpu6050.h - Prototypes for the MPU6050 accelerometer and gyroscope driver.
    //
    // Copyright (c) 2013-2017 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.1.4.178 of the Tiva Firmware Development Package.
    //
    //*****************************************************************************
    
    #ifndef __SENSORLIB_MPU6050_H__
    #define __SENSORLIB_MPU6050_H__
    
    //*****************************************************************************
    //
    // If building with a C++ compiler, make all of the definitions in this header
    // have a C binding.
    //
    //*****************************************************************************
    #ifdef __cplusplus
    extern "C"
    {
    #endif
    
    //*****************************************************************************
    //
    // The structure that defines the internal state of the MPU6050 driver.
    //
    //*****************************************************************************
    typedef struct
    {
        //
        // The pointer to the I2C master interface instance used to communicate
        // with the MPU6050.
        //
        tI2CMInstance *psI2CInst;
    
        //
        // The I2C address of the MPU6050.
        //
        uint8_t ui8Addr;
    
        //
        // The state of the state machine used while accessing the MPU6050.
        //
        uint8_t ui8State;
    
        //
        // The current accelerometer afs_sel setting.
        //
        uint8_t ui8AccelAfsSel;
    
        //
        // The new accelerometer afs_sel setting, which is used when a register
        // write succeeds.
        //
        uint8_t ui8NewAccelAfsSel;
    
        //
        // The current gyroscope fs_sel setting.
        //
        uint8_t ui8GyroFsSel;
    
        //
        // The new gyroscope fs_sel setting, which is used when a register write
        // succeeds.
        //
        uint8_t ui8NewGyroFsSel;
    
        //
        // The data buffer used for sending/receiving data to/from the MPU6050.
        //
        uint8_t pui8Data[16];
    
        //
        // The function that is called when the current request has completed
        // processing.
        //
        tSensorCallback *pfnCallback;
    
        //
        // The callback data provided to the callback function.
        //
        void *pvCallbackData;
    
        //
        // A union of structures that are used for read, write and
        // read-modify-write operations.  Since only one operation can be active at
        // a time, it is safe to re-use the memory in this manner.
        //
        union
        {
            //
            // A buffer used to store the write portion of a register read.
            //
            uint8_t pui8Buffer[2];
    
            //
            // The write state used to write register values.
            //
            tI2CMWrite8 sWriteState;
    
            //
            // The read-modify-write state used to modify register values.
            //
            tI2CMReadModifyWrite8 sReadModifyWriteState;
        }
        uCommand;
    }
    tMPU6050;
    
    //*****************************************************************************
    //
    // Function prototypes.
    //
    //*****************************************************************************
    extern uint_fast8_t MPU6050Init(tMPU6050 *psInst, tI2CMInstance *psI2CInst,
                                    uint_fast8_t ui8I2CAddr,
                                    tSensorCallback *pfnCallback,
                                    void *pvCallbackData);
    extern uint_fast8_t MPU6050Read(tMPU6050 *psInst, uint_fast8_t ui8Reg,
                                    uint8_t *pui8Data, uint_fast16_t ui16Count,
                                    tSensorCallback *pfnCallback,
                                    void *pvCallbackData);
    extern uint_fast8_t MPU6050Write(tMPU6050 *psInst, uint_fast8_t ui8Reg,
                                     const uint8_t *pui8Data,
                                     uint_fast16_t ui16Count,
                                     tSensorCallback *pfnCallback,
                                     void *pvCallbackData);
    extern uint_fast8_t MPU6050ReadModifyWrite(tMPU6050 *psInst,
                                               uint_fast8_t ui8Reg,
                                               uint_fast8_t ui8Mask,
                                               uint_fast8_t ui8Value,
                                               tSensorCallback *pfnCallback,
                                               void *pvCallbackData);
    extern uint_fast8_t MPU6050DataRead(tMPU6050 *psInst,
                                        tSensorCallback *pfnCallback,
                                        void *pvCallbackData);
    extern void MPU6050DataAccelGetRaw(tMPU6050 *psInst,
                                       uint_fast16_t *pui16AccelX,
                                       uint_fast16_t *pui16AccelY,
                                       uint_fast16_t *pui16AccelZ);
    extern void MPU6050DataAccelGetFloat(tMPU6050 *psInst, float *pfAccelX,
                                         float *pfAccelY, float *pfAccelZ);
    extern void MPU6050DataGyroGetRaw(tMPU6050 *psInst, uint_fast16_t *pui16GyroX,
                                      uint_fast16_t *pui16GyroY,
                                      uint_fast16_t *pui16GyroZ);
    extern void MPU6050DataGyroGetFloat(tMPU6050 *psInst, float *pfGyroX,
                                        float *pfGyroY, float *pfGyroZ);
    
    //*****************************************************************************
    //
    // Mark the end of the C bindings section for C++ compilers.
    //
    //*****************************************************************************
    #ifdef __cplusplus
    }
    #endif
    
    #endif // __SENSORLIB_MPU6050_H__
    
  • 很谢谢你,我才发现我的“ti”文件夹里面由这个“.c文件”,里面的函数就是可以直接用吧

  • 是的。TI有第三方库的,里面的库函数可以直接调用。

  • 能说明一下具体怎么调用嘛?

  • 第三方库在哪里?
  • C:\ti\TivaWare_C_Series-2.1.4.178\sensorlib

    TIVA下这个文件夹下就有6050的库的。