This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C 400k I2C slave spec

Other Parts Discussed in Thread: TM4C1230H6PM

请问一下TM4C1230H6PM有支援I2C 

Four transmission speeds: – Standard (100 Kbps) – Fast-mode (400 Kbps) – Fast-mode plus (1 Mbps) – High-speed mode (3.33 Mbps),

是否有明确的规格可以知道说其他IC Master(400Kbps)传送资料给TM4C Slave时。

rise time (V - - IL =0.5 V to V IH =2.4 V)

fall time (V - 9 10 ns IH =2.4 V to V IL =0.5 V)

能接收到的max 和 min各别是多少,TI规格书上只有Master的规格