This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432 SPI



板卡: MSP432P401R

因为 从设备需求,需要将MSP432  SPI 输出 clk的空闲电平为高电平, CS 空闲电平为高电平, MOSI 空闲电平为高电平, MISO空闲电平为低电平。

但我现在可以配置clk的空闲电平为高电平, CS 空闲电平为高电平。 但 MOSI 和 MISO一直为低电平。

请问该如何配置MOSI的空闲电平为高电平?? 我的SPI初始化配置如下所示:

void SR_SPI_Init(void){
volatile uint32_t delay;
EUSCI_A3->CTLW0 = 0x0001; // hold the eUSCI module in reset mode


EUSCI_A3->CTLW0 = 0x6D83;

EUSCI_A3->BRW = 10000; //8 -- 1500kHz

EUSCI_A3->MCTLW = 0;

P9->SEL0 |= 0xF0;
P9->SEL1 &= ~0xF0; // configure P9.7, P9.6, P9.5, and P9.4 as primary module function


EUSCI_A3->CTLW0 &= ~0x0001; // enable eUSCI module
EUSCI_A3->IE &= ~0x0003; // disable interrupts


}

  • 您可以看一下

    dev.ti.com/.../group__spi__api.html

    没有可以直接配置的

    您可以尝试在其空闲时配置成IO 输出高电平
  • 您好,

    需要一个MSP432 SPI 异步通信的API 或配置寄存器的方法。

    您那边可以提供一下吗?
  • 有相关寄存器的,您可以看一下 www.ti.com.cn/.../slau356h.pdf 的25.5.1 UCBxCTLW0 Register
  • SPI所有可配置的项可以查看库函数。

    /*
     * -------------------------------------------
     *    MSP432 DriverLib - v3_21_00_05 
     * -------------------------------------------
     *
     * --COPYRIGHT--,BSD,BSD
     * Copyright (c) 2016, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    #ifndef SPI_H_
    #define SPI_H_
    
    //*****************************************************************************
    //
    //! \addtogroup spi_api
    //! @{
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // If building with a C++ compiler, make all of the definitions in this header
    // have a C binding.
    //
    //*****************************************************************************
    #ifdef __cplusplus
    extern "C"
    {
    #endif
    
    #include <stdbool.h>
    #include <stdint.h>
    #include <msp.h>
    #include "eusci.h"
    
    /* Configuration Defines */
    #define EUSCI_SPI_CLOCKSOURCE_ACLK    EUSCI_B_CTLW0_SSEL__ACLK
    #define EUSCI_SPI_CLOCKSOURCE_SMCLK   EUSCI_B_CTLW0_SSEL__SMCLK
    
    #define EUSCI_SPI_MSB_FIRST    EUSCI_B_CTLW0_MSB
    #define EUSCI_SPI_LSB_FIRST    0x00
    
    #define EUSCI_SPI_BUSY        EUSCI_A_STATW_BUSY
    #define EUSCI_SPI_NOT_BUSY    0x00
    
    #define EUSCI_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT    0x00
    #define EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT    EUSCI_B_CTLW0_CKPH
    
    #define EUSCI_SPI_3PIN                      EUSCI_B_CTLW0_MODE_0
    #define EUSCI_SPI_4PIN_UCxSTE_ACTIVE_HIGH   EUSCI_B_CTLW0_MODE_1
    #define EUSCI_SPI_4PIN_UCxSTE_ACTIVE_LOW    EUSCI_B_CTLW0_MODE_2
    
    #define EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_HIGH    EUSCI_B_CTLW0_CKPL
    #define EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_LOW     0x00
    
    #define EUSCI_SPI_TRANSMIT_INTERRUPT    EUSCI_B__TXIE
    #define EUSCI_SPI_RECEIVE_INTERRUPT     EUSCI_B__RXIE
    
    #define EUSCI_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE           EUSCI_B_CTLW0_STEM
    #define EUSCI_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS    0x00
    
    //*****************************************************************************
    //
    //!     ypedef eUSCI_SPI_MasterConfig
    //! \brief Type definition for \link _eUSCI_SPI_MasterConfig \endlink structure
    //!
    //! \struct _eUSCI_SPI_MasterConfig
    //! \brief Configuration structure for master mode in the \b SPI module. See
    //!          \link SPI_initMaster \endlink for parameter documentation.
    //
    //*****************************************************************************
    typedef struct _eUSCI_SPI_MasterConfig
    {
        uint_fast8_t selectClockSource;
        uint32_t clockSourceFrequency;
        uint32_t desiredSpiClock;
        uint_fast16_t msbFirst;
        uint_fast16_t clockPhase;
        uint_fast16_t clockPolarity;
        uint_fast16_t spiMode;
    } eUSCI_SPI_MasterConfig;
    
    //*****************************************************************************
    //
    //!     ypedef eUSCI_SPI_SlaveConfig
    //! \brief Type definition for \link _eUSCI_SPI_SlaveConfig \endlink structure
    //!
    //! \struct _eUSCI_SPI_SlaveConfig
    //! \brief Configuration structure for slave mode in the \b SPI module. See
    //!          \link SPI_initSlave \endlink for parameter documentation.
    //
    //*****************************************************************************
    typedef struct _eUSCI_SPI_SlaveConfig
    {
        uint_fast16_t msbFirst;
        uint_fast16_t clockPhase;
        uint_fast16_t clockPolarity;
        uint_fast16_t spiMode;
    } eUSCI_SPI_SlaveConfig;
    
    //*****************************************************************************
    //
    //! Initializes the SPI Master block.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //! \param config Configuration structure for SPI master mode
    //!
    //! <hr>
    //! <b>Configuration options for \link eUSCI_SPI_MasterConfig \endlink structure.</b>
    //! <hr>
    //!
    //! \param selectClockSource selects clock source. Valid values are
    //!         - \b  EUSCI_SPI_CLOCKSOURCE_ACLK
    //!         - \b  EUSCI_SPI_CLOCKSOURCE_SMCLK
    //! \param clockSourceFrequency is the frequency of the selected clock source
    //! \param desiredSpiClock is the desired clock rate for SPI communication
    //! \param msbFirst controls the direction of the receive and transmit shift
    //!      register. Valid values are
    //!         - \b  EUSCI_SPI_MSB_FIRST
    //!         - \b  EUSCI_SPI_LSB_FIRST [Default Value]
    //! \param clockPhase is clock phase select.
    //!         Valid values are
    //!         - \b  EUSCI_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT
    //!                                                          [Default Value]
    //!         - \b  EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT
    //! \param clockPolarity is clock polarity select.
    //!         Valid values are
    //!         - \b  EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_HIGH
    //!         - \b  EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_LOW  [Default Value]
    //! \param spiMode is SPI mode select.
    //!         Valid values are
    //!         - \b  EUSCI_SPI_3PIN [Default Value]
    //!         - \b  EUSCI_SPI_4PIN_UCxSTE_ACTIVE_HIGH
    //!         - \b  EUSCI_SPI_4PIN_UCxSTE_ACTIVE_LOW
    //! Upon successful initialization of the SPI master block, this function
    //! will have set the bus speed for the master, but the SPI Master block
    //! still remains disabled and must be enabled with SPI_enableModule()
    //!
    //! Modified bits are \b UCCKPH, \b UCCKPL, \b UC7BIT, \b UCMSB,\b UCSSELx,
    //! \b UCSWRST bits of \b UCAxCTLW0 register
    //!
    //! \return true
    //
    //*****************************************************************************
    extern bool SPI_initMaster(uint32_t moduleInstance,
            const eUSCI_SPI_MasterConfig *config);
    
    //*****************************************************************************
    //
    //! Selects 4Pin Functionality
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param select4PinFunctionality selects Clock source. Valid values are
    //!         - \b EUSCI_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS
    //!         - \b EUSCI_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE
    //! This function should be invoked only in 4-wire mode. Invoking this function
    //! has no effect in 3-wire mode.
    //!
    //! Modified bits are \b UCSTEM bit of \b UCAxCTLW0 register
    //!
    //! \return true
    //
    //*****************************************************************************
    extern void SPI_selectFourPinFunctionality(uint32_t moduleInstance,
            uint_fast8_t select4PinFunctionality);
    
    //*****************************************************************************
    //
    //! Initializes the SPI Master clock.At the end of this function call, SPI
    //! module is left enabled.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param clockSourceFrequency is the frequency of the selected clock source
    //! \param desiredSpiClock is the desired clock rate for SPI communication.
    //!
    //! Modified bits are \b UCSWRST bit of \b UCAxCTLW0 register and
    //! \b UCAxBRW register
    //!
    //! \return None
    //
    //*****************************************************************************
    extern void SPI_changeMasterClock(uint32_t moduleInstance,
            uint32_t clockSourceFrequency, uint32_t desiredSpiClock);
    
    //*****************************************************************************
    //
    //! Initializes the SPI Slave block.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //! \param config Configuration structure for SPI slave mode
    //!
    //! <hr>
    //! <b>Configuration options for \link eUSCI_SPI_SlaveConfig \endlink structure.</b>
    //! <hr>
    //!
    //! \param msbFirst controls the direction of the receive and transmit shift
    //!      register. Valid values are
    //!         - \b  EUSCI_SPI_MSB_FIRST
    //!         - \b  EUSCI_SPI_LSB_FIRST [Default Value]
    //! \param clockPhase is clock phase select.
    //!         Valid values are
    //!         - \b  EUSCI_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT
    //!                                                          [Default Value]
    //!         - \b  EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT
    //! \param clockPolarity is clock polarity select.
    //!         Valid values are
    //!         - \b  EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_HIGH
    //!         - \b  EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_LOW [Default Value]
    //! \param spiMode is SPI mode select.
    //!         Valid values are
    //!         - \b  EUSCI_SPI_3PIN [Default Value]
    //!         - \b  EUSCI_SPI_4PIN_UCxSTE_ACTIVE_HIGH
    //!         - \b  EUSCI_SPI_4PIN_UCxSTE_ACTIVE_LOW
    //! Upon successful initialization of the SPI slave block, this function
    //! will have initialized the slave block, but the SPI Slave block
    //! still remains disabled and must be enabled with SPI_enableModule()
    //!
    //! Modified bits are \b UCMSB, \b UC7BIT, \b UCMST, \b UCCKPL, \b UCCKPH,
    //! \b UCMODE, \b UCSWRST bits of \b UCAxCTLW0
    //!
    //! \return true
    //*****************************************************************************
    extern bool SPI_initSlave(uint32_t moduleInstance,
            const eUSCI_SPI_SlaveConfig *config);
    
    //*****************************************************************************
    //
    //! Changes the SPI clock phase and polarity.At the end of this function call,
    //! SPI module is left enabled.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param clockPhase is clock phase select.
    //!         Valid values are:
    //!             - \b EUSCI_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT
    //!                                                          [Default Value]
    //!             - \b EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT
    //! \param clockPolarity is clock polarity select.
    //!         Valid values are:
    //!             - \b EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_HIGH
    //!             - \b EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_LOW  [Default Value]
    //!
    //! Modified bits are \b UCSWRST, \b UCCKPH, \b UCCKPL, \b UCSWRST bits of
    //! \b UCAxCTLW0
    //!
    //! \return None
    //
    //*****************************************************************************
    extern void SPI_changeClockPhasePolarity(uint32_t moduleInstance,
            uint_fast16_t clockPhase, uint_fast16_t clockPolarity);
    
    //*****************************************************************************
    //
    //! Transmits a byte from the SPI Module.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param transmitData data to be transmitted from the SPI module
    //!
    //! This function will place the supplied data into SPI transmit data register
    //! to start transmission
    //!
    //! Modified register is \b UCAxTXBUF
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_transmitData(uint32_t moduleInstance,
            uint_fast8_t transmitData);
    
    //*****************************************************************************
    //
    //! Receives a byte that has been sent to the SPI Module.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //!
    //! This function reads a byte of data from the SPI receive data Register.
    //!
    //! \return Returns the byte received from by the SPI module, cast as an
    //! uint8_t.
    //
    //*****************************************************************************
    extern uint8_t SPI_receiveData(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Enables the SPI block.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //!
    //! This will enable operation of the SPI block.
    //! Modified bits are \b UCSWRST bit of \b UCAxCTLW0 register.
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_enableModule(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Disables the SPI block.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //!
    //! This will disable operation of the SPI block.
    //!
    //! Modified bits are \b UCSWRST bit of \b UCAxCTLW0 register.
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_disableModule(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Returns the address of the RX Buffer of the SPI for the DMA module.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //!
    //! Returns the address of the SPI RX Buffer. This can be used in conjunction
    //! with the DMA to store the received data directly to memory.
    //!
    //! \return NONE
    //
    //*****************************************************************************
    extern uint32_t SPI_getReceiveBufferAddressForDMA(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Returns the address of the TX Buffer of the SPI for the DMA module.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //!
    //! Returns the address of the SPI TX Buffer. This can be used in conjunction
    //! with the DMA to obtain transmitted data directly from memory.
    //!
    //! \return NONE
    //
    //*****************************************************************************
    extern uint32_t SPI_getTransmitBufferAddressForDMA(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Indicates whether or not the SPI bus is busy.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //!
    //! This function returns an indication of whether or not the SPI bus is
    //! busy.This function checks the status of the bus via UCBBUSY bit
    //!
    //! \return EUSCI_SPI_BUSY if the SPI module transmitting or receiving
    //! is busy; otherwise, returns EUSCI_SPI_NOT_BUSY.
    //
    //*****************************************************************************
    extern uint_fast8_t SPI_isBusy(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Enables individual SPI interrupt sources.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param mask is the bit mask of the interrupt sources to be enabled.
    //!
    //! Enables the indicated SPI interrupt sources.  Only the sources that
    //! are enabled can be reflected to the processor interrupt; disabled sources
    //! have no effect on the processor.
    //!
    //! The mask parameter is the logical OR of any of the following:
    //!       - \b EUSCI_SPI_RECEIVE_INTERRUPT Receive interrupt
    //!       - \b EUSCI_SPI_TRANSMIT_INTERRUPT Transmit interrupt
    //!
    //! Modified registers are \b UCAxIFG and \b UCAxIE
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_enableInterrupt(uint32_t moduleInstance, uint_fast8_t mask);
    
    //*****************************************************************************
    //
    //! Disables individual SPI interrupt sources.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param mask is the bit mask of the interrupt sources to be
    //! disabled.
    //!
    //! Disables the indicated SPI interrupt sources.  Only the sources that
    //! are enabled can be reflected to the processor interrupt; disabled sources
    //! have no effect on the processor.
    //!
    //! The mask parameter is the logical OR of any of the following:
    //!       - \b EUSCI_SPI_RECEIVE_INTERRUPT Receive interrupt
    //!       - \b EUSCI_SPI_TRANSMIT_INTERRUPT Transmit interrupt
    //!
    //! Modified register is \b UCAxIE
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_disableInterrupt(uint32_t moduleInstance, uint_fast8_t mask);
    
    //*****************************************************************************
    //
    //! Gets the current SPI interrupt status.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //! \param mask Mask of interrupt to filter. This can include:
    //!          - \b EUSCI_SPI_RECEIVE_INTERRUPT -Receive interrupt
    //!          - \b EUSCI_SPI_TRANSMIT_INTERRUPT - Transmit interrupt
    //!
    //! Modified registers are \b UCAxIFG.
    //!
    //! \return The current interrupt status as the mask of the set flags
    //! Mask parameter can be either any of the following selection:
    //! - \b EUSCI_SPI_RECEIVE_INTERRUPT -Receive interrupt
    //! - \b EUSCI_SPI_TRANSMIT_INTERRUPT - Transmit interrupt
    //
    //*****************************************************************************
    extern uint_fast8_t SPI_getInterruptStatus(uint32_t moduleInstance,
            uint16_t mask);
    
    //*****************************************************************************
    //
    //! Gets the current SPI interrupt status masked with the enabled interrupts.
    //! This function is useful to call in ISRs to get a list of pending
    //! interrupts that are actually enabled and could have caused
    //! the ISR.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! Modified registers are \b UCAxIFG.
    //!
    //! \return The current interrupt status as the mask of the set flags
    //! Mask parameter can be either any of the following selection:
    //! - \b EUSCI_SPI_RECEIVE_INTERRUPT -Receive interrupt
    //! - \b EUSCI_SPI_TRANSMIT_INTERRUPT - Transmit interrupt
    //
    //*****************************************************************************
    extern uint_fast8_t SPI_getEnabledInterruptStatus(uint32_t moduleInstance);
    
    //*****************************************************************************
    //
    //! Clears the selected SPI interrupt status flag.
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! \param mask is the masked interrupt flag to be cleared.
    //!
    //! The mask parameter is the logical OR of any of the following:
    //! - \b EUSCI_SPI_RECEIVE_INTERRUPT -Receive interrupt
    //! - \b EUSCI_SPI_TRANSMIT_INTERRUPT - Transmit interrupt
    //! Modified registers are \b UCAxIFG.
    //!
    //! \return None
    //
    //*****************************************************************************
    extern void SPI_clearInterruptFlag(uint32_t moduleInstance, uint_fast8_t mask);
    
    //*****************************************************************************
    //
    //! Registers an interrupt handler for the timer capture compare interrupt.
    //!
    //! \param moduleInstance is the instance of the eUSCI (SPI) module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!  It is important to note that for eUSCI modules, only "B" modules such as
    //!  EUSCI_B0 can be used. "A" modules such as EUSCI_A0 do not support the
    //!  I2C mode.
    //!
    //! \param intHandler is a pointer to the function to be called when the
    //! timer capture compare interrupt occurs.
    //!
    //! This function registers the handler to be called when a timer
    //! interrupt occurs. This function enables the global interrupt in the
    //! interrupt controller; specific SPI interrupts must be enabled
    //! via SPI_enableInterrupt().  It is the interrupt handler's responsibility to
    //! clear the interrupt source via SPI_clearInterruptFlag().
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_registerInterrupt(uint32_t moduleInstance,
            void (*intHandler)(void));
    
    //*****************************************************************************
    //
    //! Unregisters the interrupt handler for the timer
    //!
    //! \param moduleInstance is the instance of the eUSCI A/B module. Valid
    //! parameters vary from part to part, but can include:
    //!         - \b EUSCI_A0_BASE
    //!         - \b EUSCI_A1_BASE
    //!         - \b EUSCI_A2_BASE
    //!         - \b EUSCI_A3_BASE
    //!         - \b EUSCI_B0_BASE
    //!         - \b EUSCI_B1_BASE
    //!         - \b EUSCI_B2_BASE
    //!         - \b EUSCI_B3_BASE
    //!
    //! This function unregisters the handler to be called when timer
    //! interrupt occurs.  This function also masks off the interrupt in the
    //! interrupt controller so that the interrupt handler no longer is called.
    //!
    //! \sa Interrupt_registerInterrupt() for important information about
    //! registering interrupt handlers.
    //!
    //! \return None.
    //
    //*****************************************************************************
    extern void SPI_unregisterInterrupt(uint32_t moduleInstance);
    
    /* Backwards Compatibility Layer */
    #define EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT            0x00
    #define EUSCI_B_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT          UCCKPH
    
    #define EUSCI_B_SPI_MSB_FIRST                                             UCMSB
    #define EUSCI_B_SPI_LSB_FIRST                                              0x00
    
    #define EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH                        UCCKPL
    #define EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_LOW                           0x00
    
    #define EUSCI_B_SPI_CLOCKSOURCE_ACLK                               UCSSEL__ACLK
    #define EUSCI_B_SPI_CLOCKSOURCE_SMCLK                             UCSSEL__SMCLK
    
    #define EUSCI_B_SPI_3PIN                                               UCMODE_0
    #define EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_HIGH                            UCMODE_1
    #define EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_LOW                             UCMODE_2
    
    #define EUSCI_B_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS                   0x00
    #define EUSCI_B_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE                        UCSTEM
    
    #define EUSCI_B_SPI_TRANSMIT_INTERRUPT                                   UCTXIE
    #define EUSCI_B_SPI_RECEIVE_INTERRUPT                                    UCRXIE
    
    #define EUSCI_B_SPI_BUSY                                                 UCBUSY
    #define EUSCI_B_SPI_NOT_BUSY                                               0x00
    
    #define EUSCI_A_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT            0x00
    #define EUSCI_A_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT          UCCKPH
    
    #define EUSCI_A_SPI_MSB_FIRST                                             UCMSB
    #define EUSCI_A_SPI_LSB_FIRST                                              0x00
    
    #define EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_HIGH                        UCCKPL
    #define EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_LOW                           0x00
    
    #define EUSCI_A_SPI_CLOCKSOURCE_ACLK                               UCSSEL__ACLK
    #define EUSCI_A_SPI_CLOCKSOURCE_SMCLK                             UCSSEL__SMCLK
    
    #define EUSCI_A_SPI_3PIN                                               UCMODE_0
    #define EUSCI_A_SPI_4PIN_UCxSTE_ACTIVE_HIGH                            UCMODE_1
    #define EUSCI_A_SPI_4PIN_UCxSTE_ACTIVE_LOW                             UCMODE_2
    
    #define EUSCI_A_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS                   0x00
    #define EUSCI_A_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE                        UCSTEM
    
    #define EUSCI_A_SPI_TRANSMIT_INTERRUPT                                   UCTXIE
    #define EUSCI_A_SPI_RECEIVE_INTERRUPT                                    UCRXIE
    
    #define EUSCI_A_SPI_BUSY                                                 UCBUSY
    #define EUSCI_A_SPI_NOT_BUSY                                               0x00
    
    extern void EUSCI_A_SPI_select4PinFunctionality(uint32_t baseAddress,
            uint8_t select4PinFunctionality);
    extern void EUSCI_A_SPI_masterChangeClock(uint32_t baseAddress,
            uint32_t clockSourceFrequency, uint32_t desiredSpiClock);
    extern bool EUSCI_A_SPI_slaveInit(uint32_t baseAddress, uint16_t msbFirst,
            uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode);
    extern void EUSCI_A_SPI_changeClockPhasePolarity(uint32_t baseAddress,
            uint16_t clockPhase, uint16_t clockPolarity);
    extern void EUSCI_A_SPI_transmitData(uint32_t baseAddress,
            uint8_t transmitData);
    extern uint8_t EUSCI_A_SPI_receiveData(uint32_t baseAddress);
    extern void EUSCI_A_SPI_enableInterrupt(uint32_t baseAddress, uint8_t mask);
    extern void EUSCI_A_SPI_disableInterrupt(uint32_t baseAddress, uint8_t mask);
    extern uint8_t EUSCI_A_SPI_getInterruptStatus(uint32_t baseAddress,
            uint8_t mask);
    extern void EUSCI_A_SPI_clearInterruptFlag(uint32_t baseAddress, uint8_t mask);
    extern void EUSCI_A_SPI_enable(uint32_t baseAddress);
    extern void EUSCI_A_SPI_disable(uint32_t baseAddress);
    extern uint32_t EUSCI_A_SPI_getReceiveBufferAddressForDMA(uint32_t baseAddress);
    extern uint32_t EUSCI_A_SPI_getTransmitBufferAddressForDMA(
            uint32_t baseAddress);
    extern bool EUSCI_A_SPI_isBusy(uint32_t baseAddress);
    extern void EUSCI_B_SPI_select4PinFunctionality(uint32_t baseAddress,
            uint8_t select4PinFunctionality);
    extern void EUSCI_B_SPI_masterChangeClock(uint32_t baseAddress,
            uint32_t clockSourceFrequency, uint32_t desiredSpiClock);
    extern bool EUSCI_B_SPI_slaveInit(uint32_t baseAddress, uint16_t msbFirst,
            uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode);
    extern void EUSCI_B_SPI_changeClockPhasePolarity(uint32_t baseAddress,
            uint16_t clockPhase, uint16_t clockPolarity);
    extern void EUSCI_B_SPI_transmitData(uint32_t baseAddress,
            uint8_t transmitData);
    extern uint8_t EUSCI_B_SPI_receiveData(uint32_t baseAddress);
    extern void EUSCI_B_SPI_enableInterrupt(uint32_t baseAddress, uint8_t mask);
    extern void EUSCI_B_SPI_disableInterrupt(uint32_t baseAddress, uint8_t mask);
    extern uint8_t EUSCI_B_SPI_getInterruptStatus(uint32_t baseAddress,
            uint8_t mask);
    extern void EUSCI_B_SPI_clearInterruptFlag(uint32_t baseAddress, uint8_t mask);
    extern void EUSCI_B_SPI_enable(uint32_t baseAddress);
    extern void EUSCI_B_SPI_disable(uint32_t baseAddress);
    extern uint32_t EUSCI_B_SPI_getReceiveBufferAddressForDMA(uint32_t baseAddress);
    extern uint32_t EUSCI_B_SPI_getTransmitBufferAddressForDMA(
            uint32_t baseAddress);
    extern bool EUSCI_B_SPI_isBusy(uint32_t baseAddress);
    
    //*****************************************************************************
    //
    // Mark the end of the C bindings section for C++ compilers.
    //
    //*****************************************************************************
    #ifdef __cplusplus
    }
    #endif
    
    //*****************************************************************************
    //
    // Close the Doxygen group.
    //! @}
    //
    //*****************************************************************************
    
    #endif /* SPI_H_ */