Other Parts Discussed in Thread: ADS1299EEGFE-PDK
我想要利用MSP432P401R(MASTER)寫一個可以透過spi發送命令並且接收slave回傳的數據的程式碼,我的想法是指令可以透過main迴圈裡面的SPI_transmitData(EUSCI_B0_BASE, TXData);發送,假設我有5個指令,那我可以在main透過連續5行此指令,只需更換TXData變數,然後發送給slave,並在中斷處,透過RXData = SPI_receiveData(EUSCI_B0_BASE);來接收從slave回傳的資料,但根據以下的程式碼,我的clock在示波器上顯示為'3.3V的一條直線,完全沒有嬰出現的波行,我不懂發生了什麼事?麻煩給予指教謝謝!
/* --COPYRIGHT--,BSD
* Copyright (c) 2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
/******************************************************************************
* MSP432 SPI - 3-wire Master Incremented Data
*
* This example shows how SPI master talks to SPI slave using 3-wire mode.
* Incrementing data is sent by the master starting at 0x01. Received data is
* expected to be same as the previous transmission. eUSCI RX ISR is used to
* handle communication with the CPU, normally in LPM0. Because all execution
* after LPM0 is in ISRs, initialization waits for DCO to stabilize against
* ACLK.
*
* Note that in this example, EUSCIB0 is used for the SPI port. If the user
* wants to use EUSCIA for SPI operation, they are able to with the same APIs
* with the EUSCI_AX parameters.
*
* ACLK = ~32.768kHz, MCLK = SMCLK = DCO 3MHz
*
* Use with SPI Slave Data Echo code example.
*
* MSP432P401
* -----------------
* | |
* | |
* | |
* | P1.6|-> Data Out (UCB0SIMO)
* | |
* | P1.7|<- Data In (UCB0SOMI)
* | |
* | P1.5|-> Serial Clock Out (UCB0CLK)
*******************************************************************************/
/* DriverLib Includes */
#include <ti/devices/msp432p4xx/driverlib/driverlib.h>
/* Standard Includes */
#include <stdint.h>
#include <stdbool.h>
/* Statics */
static volatile uint8_t RXData = 0;
static uint8_t TXData = 0;
//![Simple SPI Config]
/* SPI Master Configuration Parameter */
const eUSCI_SPI_MasterConfig spiMasterConfig =
{
EUSCI_B_SPI_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
3000000, // SMCLK = DCO = 3MHZ
500000, // *** = 500khz
EUSCI_B_SPI_MSB_FIRST, // MSB First
EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, // Phase
EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, // High polarity
EUSCI_B_SPI_3PIN // 3Wire SPI Mode
};
//![Simple SPI Config]
int main(void)
{
/* Halting WDT */
WDT_A_holdTimer();
//![Simple SPI Example]
/* Selecting P1.5 P1.6 and P1.7 in SPI mode */
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
/* Configuring SPI in 3wire master mode */
SPI_initMaster(EUSCI_B0_BASE, &spiMasterConfig);
/* Enable SPI module */
SPI_enableModule(EUSCI_B0_BASE);
/* Enabling interrupts */
SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT);
Interrupt_enableInterrupt(INT_EUSCIB0);
Interrupt_enableSleepOnIsrExit();
//![Simple SPI Example]
TXData = 0x01;
/* Polling to see if the TX buffer is ready */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
/* Transmitting data to slave */
SPI_transmitData(EUSCI_B0_BASE, TXData);
PCM_gotoLPM0();
__no_operation();
}
//******************************************************************************
//
//This is the EUSCI_B0 interrupt vector service routine.
//
//******************************************************************************
void EUSCIB0_IRQHandler(void)
{
uint32_t status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);
uint32_t jj;
SPI_clearInterruptFlag(EUSCI_B0_BASE, status);
if(status & EUSCI_B_SPI_RECEIVE_INTERRUPT)
{
/* USCI_B0 TX buffer ready? */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE, EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
RXData = SPI_receiveData(EUSCI_B0_BASE);
/* Send the next data packet */
//SPI_transmitData(EUSCI_B0_BASE, ++TXData);
/* Delay between transmissions for slave to process information */
//for(jj=50;jj<50;jj++);
}
}