This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430的ADC12,采用单通道多次采样的模式,未开中断,请问:第一,ad转换完成后,如果上次转换结果未读取,本次转换结果是否覆盖原有数据?第二,结果是否存放在ADC12MEM0?

Other Parts Discussed in Thread: MSP430FG4618

MSP430的ADC12,采用单通道多次采样的模式,未开中断,请问:第一,ad转换完成后,如果上次转换结果未读取,本次转换结果是否覆盖原有数据?第二,结果是否存放在ADC12MEM0?

  • 请问您现在使用的芯片具体型号是什么?

    1 当ADC12MEMx中原有数据还没有读出,而又有新的转换结果数据要写入时,则发生溢出

    2 是的,ADC12MEMx是用于存放转换结果的
  • 谢谢,请问下面代码有问题吗

    通道7

    P6SEL |= 0x80;                            // ADC sampled on P6.7
       
        ADC12CTL0 &= ~ENC;                      //ADC12CTL0  page807
        ADC12CTL0 &= ~(REFON | ADC12SC);
        ADC12CTL0 = ADC12ON|SHT0_2;               // turn on ADC12
                                                // Sample and hold for 16 ADC12CLK cycles
        ADC12CTL1 &= ~ISSH;
        ADC12CTL1 |= (SHP | CONSEQ_2 | ADC12SSEL0 | ADC12DIV_0 | SHS_0 | CSTARTADD_0); //单通道多次采样                         // Use sampling timer

        ADC12MCTL0 |= (SREF_5 | INCH_7);                      // Vr+=VREF+ (external) & Vr- = VREF-;Channel 7

        ADC12CTL0 |= ENC;                         // Enable conversions
       
        ADC12CTL0 |= ADC12SC;                   // Start conversions

  • 请问是哪个芯片?我们的MSPWARE内是有ADC例程的

    http://www.ti.com/tool/MSPWARE
  • 感谢,用的MSP430FG4618
  • /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430xG461x Demo - ADC12, Repeated Single Channel Conversions
    //
    //  This example shows how to perform repeated conversions on a single channel
    //  using "repeat-single-channel" mode.  AVcc is used for the reference and
    //  repeated conversions are performed on Channel A0. Each conversion result
    //  is moved to an 8-element array called Results[].  Test by applying a
    //  voltage to channel A0, then running. To view the conversion results, open a
    //  watch window with the debugger and view Results[].
    //  ACLK = 32kHz, MCLK = SMCLK = default DCO 1048576Hz, ADC12CLK = ADC12OSC
    //
    //                MSP430xG461x
    //              ---------------
    //             |            XIN|-
    //      Vin -->|P6.0/A0        | 32kHz
    //             |           XOUT|-
    //
    //   Y. Yang
    //   Texas Instruments Inc.
    //   September 2012 
    //   Built with CCE Version: 5.2.1 and IAR Embedded Workbench Version: 6.4
    //******************************************************************************
    #include <msp430.h>
    
    volatile unsigned int Results[8];
    unsigned int Index;
    
    int main(void)
    {
      WDTCTL = WDTPW|WDTHOLD;                   // Stop watchdog timer
      P6SEL |= 0x01;                            // ADC sampled on P6.0
      ADC12CTL0 = ADC12ON|SHT0_8|MSC;           // Turn on ADC12, Sample and hold 256 ADC12CLK cycles
      ADC12CTL1 = SHP|CONSEQ_2;                 // Use sampling timer, set mode
      ADC12IE = 0x01;                           // Enable ADC12IFG.0
      ADC12CTL0 |= ENC;                         // Enable conversions
      __enable_interrupt();                     // Enable interrupts
      ADC12CTL0 |= ADC12SC;                     // Start conversion
      __bis_SR_register(LPM0_bits);             // LPM0
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = ADC12_VECTOR
    __interrupt void ADC12_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      Results[Index++] = ADC12MEM0;             // Move result, IFG is cleared
      Index &= 0x07;                            // Modulo pointer, counts up to 7 and resets
      __no_operation();                         // SET BREAKPOINT HERE
    }