Other Parts Discussed in Thread: MSP430FG4618
MSP430的ADC12,采用单通道多次采样的模式,未开中断,请问:第一,ad转换完成后,如果上次转换结果未读取,本次转换结果是否覆盖原有数据?第二,结果是否存放在ADC12MEM0?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FG4618
MSP430的ADC12,采用单通道多次采样的模式,未开中断,请问:第一,ad转换完成后,如果上次转换结果未读取,本次转换结果是否覆盖原有数据?第二,结果是否存放在ADC12MEM0?
谢谢,请问下面代码有问题吗
通道7
P6SEL |= 0x80; // ADC sampled on P6.7
ADC12CTL0 &= ~ENC; //ADC12CTL0 page807
ADC12CTL0 &= ~(REFON | ADC12SC);
ADC12CTL0 = ADC12ON|SHT0_2; // turn on ADC12
// Sample and hold for 16 ADC12CLK cycles
ADC12CTL1 &= ~ISSH;
ADC12CTL1 |= (SHP | CONSEQ_2 | ADC12SSEL0 | ADC12DIV_0 | SHS_0 | CSTARTADD_0); //单通道多次采样 // Use sampling timer
ADC12MCTL0 |= (SREF_5 | INCH_7); // Vr+=VREF+ (external) & Vr- = VREF-;Channel 7
ADC12CTL0 |= ENC; // Enable conversions
ADC12CTL0 |= ADC12SC; // Start conversions
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430xG461x Demo - ADC12, Repeated Single Channel Conversions
//
// This example shows how to perform repeated conversions on a single channel
// using "repeat-single-channel" mode. AVcc is used for the reference and
// repeated conversions are performed on Channel A0. Each conversion result
// is moved to an 8-element array called Results[]. Test by applying a
// voltage to channel A0, then running. To view the conversion results, open a
// watch window with the debugger and view Results[].
// ACLK = 32kHz, MCLK = SMCLK = default DCO 1048576Hz, ADC12CLK = ADC12OSC
//
// MSP430xG461x
// ---------------
// | XIN|-
// Vin -->|P6.0/A0 | 32kHz
// | XOUT|-
//
// Y. Yang
// Texas Instruments Inc.
// September 2012
// Built with CCE Version: 5.2.1 and IAR Embedded Workbench Version: 6.4
//******************************************************************************
#include <msp430.h>
volatile unsigned int Results[8];
unsigned int Index;
int main(void)
{
WDTCTL = WDTPW|WDTHOLD; // Stop watchdog timer
P6SEL |= 0x01; // ADC sampled on P6.0
ADC12CTL0 = ADC12ON|SHT0_8|MSC; // Turn on ADC12, Sample and hold 256 ADC12CLK cycles
ADC12CTL1 = SHP|CONSEQ_2; // Use sampling timer, set mode
ADC12IE = 0x01; // Enable ADC12IFG.0
ADC12CTL0 |= ENC; // Enable conversions
__enable_interrupt(); // Enable interrupts
ADC12CTL0 |= ADC12SC; // Start conversion
__bis_SR_register(LPM0_bits); // LPM0
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = ADC12_VECTOR
__interrupt void ADC12_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12_ISR (void)
#else
#error Compiler not supported!
#endif
{
Results[Index++] = ADC12MEM0; // Move result, IFG is cleared
Index &= 0x07; // Modulo pointer, counts up to 7 and resets
__no_operation(); // SET BREAKPOINT HERE
}