This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R黑板出现设备驱动无法启动代码10, 如何解决设备驱动出现黄色现感叹号,一直没找到解决办法,求解答

 我用的是win10企业版,下载了CCS10

下载之后,未在设备设备管理器中出现关于TI的驱动设备

于是根据网上步骤自己手动添加了设备驱动

但是出现如下图的问题(已经重装软件很多遍了,用虚拟机也是出现这种情况)

请问前辈们如何解决这种问题

  • 很抱歉,您的图片并未上传成功,若是可以的话,请您重新上传一下,谢谢

    请问您是如何手动添加驱动的?

    您可以不需要手动更新的,安装了CCS之后,插上板子是可以自动安装驱动的
  • 在我下载CCS软件后,我插入后板子电脑并没有任何反应,当我用CCS下载程序也显示没有连接目标板

    .添加驱动,是在win10中的设备管理器中

    点击了操作选项里的添加过时设备里添加的

  • 那请您下一下独立的XDS的驱动包来手动更新一下驱动吧

    若还是不行的话,请您尝试换一台电脑
  • win7 64位表示没有这样的问题,感觉和你的系统有很大的关系。
  • 请问如何更新独立的XDS安装包呢,之前就是因为出现问题才换的现在这台电脑,请问如果是正常情况是不是下载安装好了CCS后,在windowS的设备管理器里就不会有黄色感叹号的情况了吗
  • 是的,默认是可以自动选择CCS内包含的驱动的

    您现在可以正常识别吗?
  • 没有,还是一串黄色的感叹号。请问还有什么其他的解决办法吗,这个问题很打击我对TI设备的兴趣,我打算放弃了
  • 或者您可以把我在线诊断一下吗,这是我qq1544880381,非常感谢
  • 很抱歉给您带来的不便。

    您可以尝试如下操作,若是您安装了CCS的话

    1 设备管理器内右键点击端口

    2 选择update driver

    3 按照下图路径(即CCS内的驱动)更新一下

    我尝试右键disable了我的小红板,而后手动更新驱动并右键enable该端口,可以正常识别的

  • 若还是不行的话,那应该就是系统问题了。

    您可以试一下之前客户的解决方案

    I had a problem with the same symptoms and was able to resolve it. I don't guarantee that it will solve your problem.
    My problem stems from:
    1. The debug interface XDS110 with CMIS-DAP needs WinUSB
    2. WinUSB is installed on Windows Vista and all subsequent versions of Windows, but not Windows XP
    This is usually handled in Windows XP with a co-installer.
    TI already has some files which look like they should co-install WinUSB, so I don't know what went wrong.

    I was able to resolve it manually by using a program called zadig from http://zadig.akeo.ie/
    The procedure I followed was:
    1. Read the instructions on the web site. Read the usage guide.
    2. Download the zadig program for Windows XP and run it. Do not download the program for Vista or later.
    3. The program won't show you anything to change until you plug in the Launchpad
    4. In the selection box of the program, choose XDS110 with CMIS-DAP (the first interface);
    5. In the selection box of the program, choose XDS110 with CMIS-DAP (the second interface)
    6. Exit the program
    The device manager should say that both devices now have drivers.
    Windows may want to re-install the driver if you plug the Launchpad into a different USB port.
    The location for the driver on my installation is C:ti/ccsv6/ccs_base/emulation/windows/xds110_drivers/