Part Number: MSP432E401Y

Technical Reference似乎表示了不同的PWM Generator可以采用不同的波形频率。
然而我在使用TI-drivers时无法使不同发生器的PWM采用不同频率。我该如何解决?
此外,MSP432E4系列的产品的timer的PWM_MODE产生的波形是否有占空比为50%的限制?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E401Y

Technical Reference似乎表示了不同的PWM Generator可以采用不同的波形频率。
然而我在使用TI-drivers时无法使不同发生器的PWM采用不同频率。我该如何解决?
此外,MSP432E4系列的产品的timer的PWM_MODE产生的波形是否有占空比为50%的限制?
您是否有参考TI例程:
simplelink_msp432e4_sdk_4_20_00_12\examples\nortos\MSP_EXP432E401Y\driverlib\pwm_genx_syncgenerators

抱歉,我这边找了一下,没有MSP432E的板子,所以我是使用MSP432P系列来测试的
代码如下,不建议您在循环内打开PWM,即
/*** - custom variables end - ***/
for(int i=0;i<CONFIG_PWM_COUNT;i++){
pwmHandle[i] = PWM_open(i, pwmParams+i);
if(pwmHandle[i]==NULL){
//error: PWM did not open
//there had better a UART output
while(1);
}
而是尝试逐个打开
/*
* Copyright (c) 2015-2019, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== pwmled2.c ========
*/
/* For usleep() */
#include <unistd.h>
#include <stddef.h>
/* Driver Header files */
#include <ti/drivers/PWM.h>
/* Driver configuration */
#include "ti_drivers_config.h"
/*
* ======== mainThread ========
* Task periodically increments the PWM duty for the on board LED.
*/
void *mainThread(void *arg0)
{
/* Period and duty in microseconds */
uint16_t pwmPeriod = 3000;
uint16_t duty = 0;
uint16_t dutyInc = 100;
/* Sleep time in microseconds */
uint32_t time = 50000;
PWM_Handle pwm1 = NULL;
PWM_Handle pwm2 = NULL;
PWM_Params params;
/* Call driver init functions. */
PWM_init();
PWM_Params_init(¶ms);
params.dutyUnits = PWM_DUTY_US;
params.dutyValue = 0;
params.periodUnits = PWM_PERIOD_US;
params.periodValue = pwmPeriod;
pwm1 = PWM_open(CONFIG_PWM_0, ¶ms);
if (pwm1 == NULL) {
/* CONFIG_PWM_0 did not open */
while (1);
}
PWM_start(pwm1);
pwm2 = PWM_open(CONFIG_PWM_1, ¶ms);
if (pwm2 == NULL) {
/* CONFIG_PWM_0 did not open */
while (1);
}
PWM_start(pwm2);
/* Loop forever incrementing the PWM duty */
while (1) {
PWM_setDuty(pwm1, duty);
PWM_setDuty(pwm2, duty);
duty = (duty + dutyInc);
if (duty == pwmPeriod || (!duty)) {
dutyInc = - dutyInc;
}
usleep(time);
}
}
您可以看一下下面链接的
以及说明:
另外我之前附上的代码是MSP432P401R系列的例程