This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: SPI改了DCO频率太高,下不进程序

Part Number: MSP432P401R

  • 请问您是如何配置的?

    在 https://dev.ti.com/tirex/explore/node?node=AIt11.GE8nvJkpoVjCiItQ__z-lQYNj__LATEST 内

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2013, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP432 CODE EXAMPLE DISCLAIMER
     *
     * MSP432 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see http://www.ti.com/tool/mspdriverlib for an API functional
     * library & https://dev.ti.com/pinmux/ for a GUI approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP432P401 Demo - Device configuration for operation @ MCLK = DCO = 48MHz
    //
    //   Description: Proper device configuration to enable operation at MCLK=48MHz
    //   including:
    //   1. Configure VCORE level to 1
    //   2. Configure flash wait-state to 1
    //   3. Configure DCO frequency to 48MHz
    //   4. Ensure MCLK is sourced by DCO
    //
    //   After configuration is complete, MCLK is output to port pin P4.3.
    //
    //                MSP432P401x
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //            |             P4.3|----> MCLK
    //            |                 |
    //
    //   William Goh
    //   Texas Instruments Inc.
    //   June 2016 (updated) | November 2013 (created)
    //   Built with CCSv6.1, IAR, Keil, GCC
    //******************************************************************************
    #include "ti/devices/msp432p4xx/inc/msp.h"
    #include "stdint.h"
    
    
    void error(void);
    
    int main(void)
    {
        volatile uint32_t i;
        uint32_t currentPowerState;
    
        WDT_A->CTL = WDT_A_CTL_PW |
                     WDT_A_CTL_HOLD;            // Stop WDT
    
        P1->DIR |= BIT0;                        // P1.0 set as output
    
        /* NOTE: This example assumes the default power state is AM0_LDO.
         * Refer to  msp432p401x_pcm_0x code examples for more complete PCM
         * operations to exercise various power state transitions between active
         * modes.
         */
    
        /* Step 1: Transition to VCORE Level 1: AM0_LDO --> AM1_LDO */
    
        /* Get current power state, if it's not AM0_LDO, error out */
        currentPowerState = PCM->CTL0 & PCM_CTL0_CPM_MASK;
        if (currentPowerState != PCM_CTL0_CPM_0)
            error();
    
        while ((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
        PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_1;
        while ((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
        if (PCM->IFG & PCM_IFG_AM_INVALID_TR_IFG)
            error();                            // Error if transition was not successful
        if ((PCM->CTL0 & PCM_CTL0_CPM_MASK) != PCM_CTL0_CPM_1)
            error();                            // Error if device is not in AM1_LDO mode
    
        /* Step 2: Configure Flash wait-state to 1 for both banks 0 & 1 */
        FLCTL->BANK0_RDCTL = (FLCTL->BANK0_RDCTL & ~(FLCTL_BANK0_RDCTL_WAIT_MASK)) |
                FLCTL_BANK0_RDCTL_WAIT_1;
        FLCTL->BANK1_RDCTL  = (FLCTL->BANK0_RDCTL & ~(FLCTL_BANK1_RDCTL_WAIT_MASK)) |
                FLCTL_BANK1_RDCTL_WAIT_1;
    
        /* Step 3: Configure DCO to 48MHz, ensure MCLK uses DCO as source*/
        CS->KEY = CS_KEY_VAL ;                  // Unlock CS module for register access
        CS->CTL0 = 0;                           // Reset tuning parameters
        CS->CTL0 = CS_CTL0_DCORSEL_5;           // Set DCO to 48MHz
        /* Select MCLK = DCO, no divider */
        CS->CTL1 = (CS->CTL1 & ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK)) |
                CS_CTL1_SELM_3;
        CS->KEY = 0;                            // Lock CS module from unintended accesses
    
        /* Step 4: Output MCLK to port pin to demonstrate 48MHz operation */
        P4->DIR |= BIT3;
        P4->SEL0 |=BIT3;                        // Output MCLK
        P4->SEL1 &= ~(BIT3);
    
        while (1)                               // continuous loop
        {
            P1->OUT ^= BIT0;                    // Blink P1.0 LED
            for (i = 200000; i > 0; i--);       // Delay
        }
    }
    
    void error(void)
    {
        volatile uint32_t i;
    
        while (1)
        {
            P1->OUT ^= BIT0;
            for(i = 20000; i > 0; i--);           // Blink LED forever
        }
    }
    

    // Description: Proper device configuration to enable operation at MCLK=48MHz
    // including:
    // 1. Configure VCORE level to 1
    // 2. Configure flash wait-state to 1
    // 3. Configure DCO frequency to 48MHz
    // 4. Ensure MCLK is sourced by DCO

    1. 配置电压核心水平等级到1
    2. 配置Flash等待状态到1
    3. 配置数控时钟振荡频率到48MHz
    4. 确保主时钟MCLK的时钟源来自DCO

    另外 在更改 DCO 后,您可以将 MCLK 输出到引脚或使用 CS_getMCLK() 函数来评估 MCLK 频率。逻辑分析仪或示波器也可用于评估 SPI 通信速度。