Part Number: MSP432P401R


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问您是如何配置的?
在 https://dev.ti.com/tirex/explore/node?node=AIt11.GE8nvJkpoVjCiItQ__z-lQYNj__LATEST 内
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2013, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP432 CODE EXAMPLE DISCLAIMER
*
* MSP432 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see http://www.ti.com/tool/mspdriverlib for an API functional
* library & https://dev.ti.com/pinmux/ for a GUI approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP432P401 Demo - Device configuration for operation @ MCLK = DCO = 48MHz
//
// Description: Proper device configuration to enable operation at MCLK=48MHz
// including:
// 1. Configure VCORE level to 1
// 2. Configure flash wait-state to 1
// 3. Configure DCO frequency to 48MHz
// 4. Ensure MCLK is sourced by DCO
//
// After configuration is complete, MCLK is output to port pin P4.3.
//
// MSP432P401x
// -----------------
// /|\| |
// | | |
// --|RST |
// | P4.3|----> MCLK
// | |
//
// William Goh
// Texas Instruments Inc.
// June 2016 (updated) | November 2013 (created)
// Built with CCSv6.1, IAR, Keil, GCC
//******************************************************************************
#include "ti/devices/msp432p4xx/inc/msp.h"
#include "stdint.h"
void error(void);
int main(void)
{
volatile uint32_t i;
uint32_t currentPowerState;
WDT_A->CTL = WDT_A_CTL_PW |
WDT_A_CTL_HOLD; // Stop WDT
P1->DIR |= BIT0; // P1.0 set as output
/* NOTE: This example assumes the default power state is AM0_LDO.
* Refer to msp432p401x_pcm_0x code examples for more complete PCM
* operations to exercise various power state transitions between active
* modes.
*/
/* Step 1: Transition to VCORE Level 1: AM0_LDO --> AM1_LDO */
/* Get current power state, if it's not AM0_LDO, error out */
currentPowerState = PCM->CTL0 & PCM_CTL0_CPM_MASK;
if (currentPowerState != PCM_CTL0_CPM_0)
error();
while ((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_1;
while ((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
if (PCM->IFG & PCM_IFG_AM_INVALID_TR_IFG)
error(); // Error if transition was not successful
if ((PCM->CTL0 & PCM_CTL0_CPM_MASK) != PCM_CTL0_CPM_1)
error(); // Error if device is not in AM1_LDO mode
/* Step 2: Configure Flash wait-state to 1 for both banks 0 & 1 */
FLCTL->BANK0_RDCTL = (FLCTL->BANK0_RDCTL & ~(FLCTL_BANK0_RDCTL_WAIT_MASK)) |
FLCTL_BANK0_RDCTL_WAIT_1;
FLCTL->BANK1_RDCTL = (FLCTL->BANK0_RDCTL & ~(FLCTL_BANK1_RDCTL_WAIT_MASK)) |
FLCTL_BANK1_RDCTL_WAIT_1;
/* Step 3: Configure DCO to 48MHz, ensure MCLK uses DCO as source*/
CS->KEY = CS_KEY_VAL ; // Unlock CS module for register access
CS->CTL0 = 0; // Reset tuning parameters
CS->CTL0 = CS_CTL0_DCORSEL_5; // Set DCO to 48MHz
/* Select MCLK = DCO, no divider */
CS->CTL1 = (CS->CTL1 & ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK)) |
CS_CTL1_SELM_3;
CS->KEY = 0; // Lock CS module from unintended accesses
/* Step 4: Output MCLK to port pin to demonstrate 48MHz operation */
P4->DIR |= BIT3;
P4->SEL0 |=BIT3; // Output MCLK
P4->SEL1 &= ~(BIT3);
while (1) // continuous loop
{
P1->OUT ^= BIT0; // Blink P1.0 LED
for (i = 200000; i > 0; i--); // Delay
}
}
void error(void)
{
volatile uint32_t i;
while (1)
{
P1->OUT ^= BIT0;
for(i = 20000; i > 0; i--); // Blink LED forever
}
}
// Description: Proper device configuration to enable operation at MCLK=48MHz
// including:
// 1. Configure VCORE level to 1
// 2. Configure flash wait-state to 1
// 3. Configure DCO frequency to 48MHz
// 4. Ensure MCLK is sourced by DCO
另外 在更改 DCO 后,您可以将 MCLK 输出到引脚或使用 CS_getMCLK() 函数来评估 MCLK 频率。逻辑分析仪或示波器也可用于评估 SPI 通信速度。