Part Number: MSP432P401R
遇到与原贴类似问题,请求解答
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
代码和原始问题中给出的类似,跑出来结果基本一直。配置系统时钟MCLK为外部晶振48MHz,从P4.3输出MCLK时钟,波形周期为20.8ns,没问题。执行IO口连续翻转语句,输出波形周期在600多ns。向了解为什么只有两句IO口翻转语句就用了30多到40个时钟周期?

以下是我的测试代码:
/* --COPYRIGHT--,BSD
* Copyright (c) 2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
/******************************************************************************
* MSP432 Empty Project
*
* Description: An empty project that uses DriverLib
*
* MSP432P401
* ------------------
* /|\| |
* | | |
* --|RST |
* | |
* | |
* | |
* | |
* | |
* Author:
*******************************************************************************/
/* DriverLib Includes */
#include <ti/devices/msp432p4xx/driverlib/driverlib.h>
#include <ti/devices/msp432p4xx/inc/msp432p401r_classic.h>
#include <arm_math.h>
#include <arm_const_structs.h>
/* Standard Includes */
#include <stdint.h>
#include <stdbool.h>
int main(void)
{
/* Stop Watchdog */
MAP_WDT_A_holdTimer();
//![Simple CS Config]
/* Configuring pins for peripheral/crystal usage and LED for output */
MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_PJ,
GPIO_PIN3 | GPIO_PIN2, GPIO_PRIMARY_MODULE_FUNCTION);
MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);
/* Just in case the user wants to use the getACLK, getMCLK, etc. functions,
* let's set the clock frequency in the code.
*/
CS_setExternalClockSourceFrequency(32000,48000000);
/* Starting HFXT in non-bypass mode without a timeout. Before we start
* we have to change VCORE to 1 to support the 48MHz frequency */
MAP_PCM_setCoreVoltageLevel(PCM_VCORE1);
MAP_FlashCtl_setWaitState(FLASH_BANK0, 1);
MAP_FlashCtl_setWaitState(FLASH_BANK1, 1);
CS_startHFXT(false);
/* Initializing MCLK to HFXT (effectively 48MHz) */
MAP_CS_initClockSignal(CS_MCLK, CS_HFXTCLK_SELECT, CS_CLOCK_DIVIDER_1);
//![Simple CS Config]
P3OUT = 0x00;
P3OUT = 0x01;
P3OUT = 0x00;
P3OUT = 0x01;
P3OUT = 0x00;
P3MAP01 = 0x00;
P3MAP01 = 0x01;
P3MAP01 = 0x00;
/* Configuring SysTick to trigger at 12000000 (MCLK is 48MHz so this will
* make it toggle every 0.25s) */
MAP_SysTick_enableModule();
MAP_SysTick_setPeriod(12000000);
MAP_Interrupt_enableSleepOnIsrExit();
MAP_SysTick_enableInterrupt();
/* Enabling MASTER interrupts */
MAP_Interrupt_enableMaster();
while(1)
{
MAP_PCM_gotoLPM0();
}
}
void SysTick_Handler(void)
{
GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
}