This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: adc0采样异常

Part Number: MSP432E401Y

void ADC0SS2_IRQHandler(void)
{
    uint32_t getIntStatus;

    /* Get the interrupt status from the ADC */
    getIntStatus = MAP_ADCIntStatusEx(ADC0_BASE, true);

    /* If the interrupt status for Sequencer-2 is set the
     * clear the status and read the data */
    if((getIntStatus & ADC_INT_DMA_SS2) == ADC_INT_DMA_SS2)
    {
        /* Clear the ADC interrupt flag. */
        MAP_ADCIntClearEx(ADC0_BASE, ADC_INT_DMA_SS2);

        /* Reconfigure the channel control structure and enable the channel */
        MAP_uDMAChannelTransferSet(UDMA_CH16_ADC0_2 | UDMA_PRI_SELECT,
                                   UDMA_MODE_BASIC,
                                   (void *)&ADC0->SSFIFO2, (void *)&srcBuffer,
                                   sizeof(srcBuffer)/2);

        MAP_uDMAChannelEnable(UDMA_CH16_ADC0_2);

        /* Set conversion flag to true */
        bgetConvStatus = true;
    }
}

void ConfigureUART(uint32_t systemClock)
{
    /* Enable the clock to GPIO port A and UART 0 */
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

    /* Configure the GPIO Port A for UART 0 */
    MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
    MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
    MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    /* Configure the UART for 115200 bps 8-N-1 format */
    UARTStdioConfig(0, 115200, systemClock);
}

int main(void)
{
    uint32_t systemClock;
		uint32_t i=0;
    /* Configure the system clock for 120 MHz */
    systemClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN |
                                          SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480),
                                          120000000);
		
	
    /* Initialize serial console */
    ConfigureUART(systemClock);

    /* Enable the clock to GPIO Port E and wait for it to be ready */
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOE)))
    {
    }

    /* Configure PE0-PE3 as ADC input channel */
    MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
    MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2);
    MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1);
    MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0);

    /* Enable the clock to ADC-0 and wait for it to be ready */
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
    while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0)))
    {
    }

    /* Configure Sequencer 2 to sample the analog channel : AIN0-AIN3. The
     * end of conversion and interrupt generation is set for AIN3 */
    MAP_ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH3 | ADC_CTL_IE |
                                 ADC_CTL_END);
		
    /* Enable sample sequence 2 with a timer signal trigger.  Sequencer 2
     * will do a single sample when the timer generates a trigger on timeout*/
    MAP_ADCSequenceConfigure(ADC0_BASE, 2, ADC_TRIGGER_TIMER, 2);
		
		ADC0->CC=0x0;
		
    /* Clear the interrupt status flag before enabling. This is done to make
     * sure the interrupt flag is cleared before we sample. */
    MAP_ADCIntClearEx(ADC0_BASE, ADC_INT_DMA_SS2);
    MAP_ADCIntEnableEx(ADC0_BASE, ADC_INT_DMA_SS2);

    /* Enable the DMA request from ADC0 Sequencer 2 */
    MAP_ADCSequenceDMAEnable(ADC0_BASE, 2);

    /* Since sample sequence 2 is now configured, it must be enabled. */
    MAP_ADCSequenceEnable(ADC0_BASE, 2);

    /* Enable the Interrupt generation from the ADC-0 Sequencer */
    MAP_IntEnable(INT_ADC0SS2);

    /* Enable the DMA and Configure Channel for TIMER0A for Ping Pong mode of
     * transfer */
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
    while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_UDMA)))
    {
    }

    MAP_uDMAEnable();

    /* Point at the control table to use for channel control structures. */
    MAP_uDMAControlBaseSet(pui8ControlTable);

    /* Map the ADC0 Sequencer 2 DMA channel */
    MAP_uDMAChannelAssign(UDMA_CH16_ADC0_2);

    /* Put the attributes in a known state for the uDMA ADC0 Sequencer 2
     * channel. These should already be disabled by default. */
    MAP_uDMAChannelAttributeDisable(UDMA_CH16_ADC0_2,
                                    UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    /* Configure the control parameters for the primary control structure for
     * the ADC0 Sequencer 2 channel. The primary control structure is used for
     * copying the data from ADC0 Sequencer 2 FIFO to srcBuffer. The transfer
     * data size is 16 bits and the source address is not incremented while
     * the destination address is incremented at 16-bit boundary.
     */
    MAP_uDMAChannelControlSet(UDMA_CH16_ADC0_2 | UDMA_PRI_SELECT,
                              UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 |
                              UDMA_ARB_4);

    /* Set up the transfer parameters for the ADC0 Sequencer 2 primary control
     * structure. The mode is Basic mode so it will run to completion. */
    MAP_uDMAChannelTransferSet(UDMA_CH16_ADC0_2 | UDMA_PRI_SELECT,
                               UDMA_MODE_BASIC,
                               (void *)&ADC0->SSFIFO2, (void *)&srcBuffer,
                               sizeof(srcBuffer)/4);

    /* The uDMA ADC0 Sequencer 2 channel is primed to start a transfer. As
     * soon as the channel is enabled and the Timer will issue an ADC trigger,
     * the ADC will perform the conversion and send a DMA Request. The data
     * transfers will begin. */
    MAP_uDMAChannelEnable(UDMA_CH16_ADC0_2);

    /* Enable Timer-0 clock and configure the timer in periodic mode with
     * a frequency of 1 KHz. Enable the ADC trigger generation from the
     * timer-0. */
    MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
    while(!(MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER0)))
    {
    }

    MAP_TimerConfigure(TIMER0_BASE, TIMER_CFG_A_PERIODIC_UP);
    MAP_TimerLoadSet(TIMER0_BASE, TIMER_A, (systemClock/10000));
    MAP_TimerADCEventSet(TIMER0_BASE, TIMER_ADC_TIMEOUT_A);
    MAP_TimerControlTrigger(TIMER0_BASE, TIMER_A, true);
    MAP_TimerEnable(TIMER0_BASE, TIMER_A);

    /* Wait loop */
    while(1)
    {
        /* Wait for the conversion to complete */
        while(!bgetConvStatus);
        bgetConvStatus = false;

        /* Display the AIN0-AIN03 (PE3-PE0) digital value on the console. */
        for(i=0;i<1024;++i){
						UARTprintf("%d:%d\n",i,srcBuffer[i]);
				}
				MAP_SysCtlDelay(systemClock / 4);
    }
}

代码是在adc timertrigger dma例程基础上修改的

其中添加了ADC0->CC=0x0;语句 将adc0的采样来源改为pll (32m)为了达到2m采样率

但是采样出来的数据非常奇怪 采集gnd的数据为1023 采集3.3v的数据为2806

想知道除了修改adc0的寄存器还需要改动哪里才能获得2m的采样率