This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: MSP432P401R: ADC用DMA传输数据只传输了一次就会停止

Part Number: MSP432E401Y


   MAP_ADC14_enableModule();                                                                 //使能ADC14模块
    MAP_ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_3, ADC_NOROUTE); //初始化ADC 时钟 分频  通道 9.6MHz

    MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5, GPIO_PIN5, GPIO_TERTIARY_MODULE_FUNCTION); //模拟输入(p5.5 A0)
    MAP_ADC14_configureSingleSampleMode(ADC_MEM0, true);                                                    //单通道配置 多次转化true
    MAP_ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_AVCC_VREFNEG_VSS, ADC_INPUT_A0, false);       //使用内部电源电压参考 非差分输入false
    MAP_ADC14_enableInterrupt(ADC_INT0);                                                                    //ADC通道0的中断

    /* Configuring DMA module */
    MAP_DMA_enableModule();
    MAP_DMA_setControlBase(controlTable);

    /*
    * Primary DMA Channel, ADC12C
    * Size = 16bits
    * Source Increment = 16bits
    * Destination Increment = 16bits
    * Arbitration = 1 , no other sources
    */

    MAP_DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH7_ADC14,
                              UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);

    MAP_DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH7_ADC14,
                               UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[0],
                               (void*)adc_v,1024);

    //UDMA_MODE_PINGPONG    UDMA_MODE_AUTO   UDMA_MODE_BASIC
    /* Assigning/Enabling Interrupts */
    MAP_DMA_assignInterrupt(DMA_INT1, 7);
    MAP_Interrupt_enableInterrupt(INT_DMA_INT1);
    MAP_DMA_assignChannel(DMA_CH7_ADC14);
    MAP_DMA_clearInterruptFlag(7);
    MAP_Interrupt_enableMaster();

    /* Now that the DMA is primed and setup, enabling the channels. The ADC14
    * hardware should take over and transfer/receive all bytes.The DMA is
    * triggered after the conversion in single-channel conversion mode or
    * after the completion of a sequence of channel conversions in
    * sequence-ofchannels conversion mode. */
    MAP_DMA_enableChannel(7);

    /* Setting up the sample timer to automatically step through the sequence
    * convert.
    */
    ADC14_enableSampleTimer(ADC_AUTOMATIC_ITERATION);

    /* Triggering the start of the sample */
    MAP_ADC14_enableConversion();
    MAP_ADC14_toggleConversionTrigger();

  • 你好,原贴中工程师贴出的代码有参考吗?按照代码编写还是会有上述问题?

  • 是的,一直有问题,中断一直卡在里面

  • 我是参考的MSP432P401R: ADC用DMA传输数据只传输了一次就会停止 - 其他微控制器论坛 - 其他微控制器 - E2ETm 设计支持 (ti.com)的问题,但是仍然没有解决,使用的是第二个示例使用脉冲采样模式  1Msps (也使用 DMA)。 

  • 我们这边不希望是按键触发DMA,而是其他自动方式触发DMA请问有解决方案吗

    /*
     * -------------------------------------------
     *    MSP432 DriverLib - v3_10_00_09 
     * -------------------------------------------
     *
     * --COPYRIGHT--,BSD,BSD
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    /*******************************************************************************
     * MSP432 ADC14 - Single Channel Continuous Sample w/ Timer_A Trigger
     *
     * Description: In this ADC14 code example, a single input channel is sampled
     * using the standard 3.3v reference. The source of the sample trigger for this
     * example is Timer_A CCR1. The ADC is setup to continuously sample/convert
     * from A0 when the trigger starts and store the results in resultsBuffer (it
     * is setup to be a circular buffer where resPos overflows to 0). Timer_A, CCR0
     * and CCR1 are configured to generate a PWM. The CCR0 value is 23 and CCR1 is
     * set to 11, resulting in a PWM of 1us period.  The sample time is driven by
     * the ADC clock and not the PWM duty cycle.
     *
     * The PWM is started once the GPIO interrupt for P1.1 is serviced.
     *
     *                MSP432P401
     *             ------------------
     *         /|\|                  |
     *          | |                  |
     *          --|RST         P5.5  |<--- A0 (Analog Input)
     *            |                  |
     *            |            P1.1  |<--- GPIO trigger to Start conversions
     *            |                  |
     *            |            P1.0  |---> Debug port to show DMA ISR
     *            |            P2.4  |---> Debug TA0.1, ADC trigger
     *            |                  |
     *
     * Author: Timothy Logan/ C. Sterzik
     ******************************************************************************/
    /* DriverLib Includes */
    #include "driverlib.h"
    
    /* Standard Includes */
    #include <stdint.h>
    #include <stdbool.h>
    
    #define ARRAY_LENGTH	256
    
    /*
     * Timer_A Compare Configuration Parameter
     * CCR1 is used to trigger the ADC14, conversion time
     * is defined by the resolution
     * 14bit -> 16 cycles + 1 cycle (SLAU356d, 20.2.8.3)
     * 12bit -> 14 cycles + 1 cycle
     * 10bit -> 11 cycles + 1 cycle
     *  8bit ->  9 cycles + 1 cycle
     *
     *  In this example, 14-bit resolution at 24Mhz ~708ns conversion time
     *  Sample time is defined by 4 ADC clocks
     *  Sample period is 24/24Mhz = 1us
     */
    const Timer_A_PWMConfig timerA_PWM =
    {
        .clockSource = TIMER_A_CLOCKSOURCE_SMCLK,
        .clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1,
        .timerPeriod = 23,
        .compareRegister = TIMER_A_CAPTURECOMPARE_REGISTER_1,
        .compareOutputMode TIMER_A_OUTPUTMODE_SET_RESET,
        .dutyCycle = 11
    };
    
    /* DMA Control Table */
    #if defined(__TI_COMPILER_VERSION__)
    #pragma DATA_ALIGN(MSP_EXP432P401RLP_DMAControlTable, 1024)
    #elif defined(__IAR_SYSTEMS_ICC__)
    #pragma data_alignment=1024
    #elif defined(__GNUC__)
    __attribute__ ((aligned (1024)))
    #elif defined(__CC_ARM)
    __align(1024)
    #endif
    static DMA_ControlTable MSP_EXP432P401RLP_DMAControlTable[16];
    
    /* Statics */
    static volatile uint16_t resultsBufferPrimary[ARRAY_LENGTH];
    static volatile uint16_t resultsBufferAlternate[ARRAY_LENGTH];
    
    int main(void)
    {
        /* Halting WDT  */
        MAP_WDT_A_holdTimer();
        MAP_Interrupt_enableSleepOnIsrExit();
    
        /* Starting HFXT in non-bypass mode without a timeout. Before we start
          * we have to change VCORE to 1 to support the 48MHz frequency */
        MAP_PCM_setCoreVoltageLevel(PCM_VCORE1);
        MAP_FlashCtl_setWaitState(FLASH_BANK0, 1);
        MAP_FlashCtl_setWaitState(FLASH_BANK1, 1);
    
        /*
         * Setting up clocks
         * MCLK = MCLK = 48MHz
         * SMCLK = MCLK/2 = 24Mhz
         * ACLK = REFO = 32Khz
         */
        MAP_CS_setDCOFrequency(48000000);
        MAP_CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);
        MAP_CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_2);
        MAP_CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);
    
        /* Initializing ADC (SMCLK/1/1) */
        MAP_ADC14_enableModule();
        MAP_ADC14_initModule(ADC_CLOCKSOURCE_SMCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_1,
                0);
    
        /*
         * Debug
         * Configuring P1.0 as output
         */
        MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);
        P1OUT &= ~BIT0;
    
        /*
         * Configuring GPIOs (5.5 A0)
         */
        MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5, GPIO_PIN5,
        GPIO_TERTIARY_MODULE_FUNCTION);
    
        /*
         * Debug: set TA0.1 as output to see ADC trigger signal
         */
        MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN4,
        GPIO_PRIMARY_MODULE_FUNCTION);
    
        /*
         * Configuring P1.1 as an input and enabling interrupt, the timer is started from
         * GPIO ISR.
         */
        MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1);
        MAP_GPIO_interruptEdgeSelect(GPIO_PORT_P1,GPIO_PIN1,GPIO_HIGH_TO_LOW_TRANSITION);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, GPIO_PIN1);
        MAP_GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1);
    
        /*
         * Configuring ADC Memory, repeat-single-channel, A0
         */
        MAP_ADC14_configureSingleSampleMode(ADC_MEM0, true);
        /*
         * Configuring ADC Memory, reference, and single ended conversion
         * A0 goes to mem0, AVcc is the reference, and the conversion is
         * single-ended
         */
        MAP_ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_AVCC_VREFNEG_VSS,
        ADC_INPUT_A0, false);
        /*
         * Configuring the sample trigger to be sourced from Timer_A0 CCR1 and on the
         * rising edge, default samplemode is extended (SHP=0)
         */
        MAP_ADC14_setSampleHoldTrigger(ADC_TRIGGER_SOURCE1, false);
    
        /* Enabling the interrupt when a conversion on channel 1 is complete and
         * enabling conversions */
        MAP_ADC14_enableInterrupt(ADC_INT0);
        MAP_ADC14_enableConversion();
    
        /* Configuring DMA module */
        MAP_DMA_enableModule();
        MAP_DMA_setControlBase(MSP_EXP432P401RLP_DMAControlTable);
    
        /*
         * Setup the DMA + ADC14 interface
         */
        MAP_DMA_disableChannelAttribute(DMA_CH7_ADC14,
                                     UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                     UDMA_ATTR_HIGH_PRIORITY |
                                     UDMA_ATTR_REQMASK);
    
        /*
         * Setting Control Indexes. In this case we will set the source of the
         * DMA transfer to ADC14 Memory 0 and the destination to the destination
         * data array.
         */
        MAP_DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH7_ADC14,
        		UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
        MAP_DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH7_ADC14,
        		UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[0],
    			(void*)resultsBufferPrimary, ARRAY_LENGTH);
        MAP_DMA_setChannelControl(UDMA_ALT_SELECT | DMA_CH7_ADC14,
        		UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
        MAP_DMA_setChannelTransfer(UDMA_ALT_SELECT | DMA_CH7_ADC14,
        		UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[0],
    			(void*)resultsBufferAlternate, ARRAY_LENGTH);
    
        /* Assigning/Enabling Interrupts */
        MAP_DMA_assignInterrupt(DMA_INT1, 7);
        MAP_DMA_assignChannel(DMA_CH7_ADC14);
        MAP_DMA_clearInterruptFlag(7);
    
        /* Enabling Interrupts */
        MAP_Interrupt_enableInterrupt(INT_DMA_INT1);
        MAP_Interrupt_enableInterrupt(INT_PORT1);
        MAP_Interrupt_enableMaster();
    
        /* Going to sleep */
        MAP_PCM_gotoLPM0();
        __no_operation();
    }
    
    /* Completion interrupt for ADC14 MEM0 */
    __attribute__((ramfunc))  // Requires compiler TI v15.12.1.LTS
    void DMA_INT1_IRQHandler(void)
    {
    	MAP_Timer_A_stopTimer(TIMER_A0_BASE);
        MAP_DMA_disableChannel(7);
        P1->OUT |= BIT0;
        /*
         * Switch between primary and alternate bufferes with DMA's PingPong mode
         */
        if (MAP_DMA_getChannelAttribute(7) & UDMA_ATTR_ALTSELECT)
        {
    //        MAP_DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH7_ADC14,
    //        		UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    //        MAP_DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH7_ADC14,
    //        		UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[0],
    //    			resultsBufferPrimary, ARRAY_LENGTH);
        	MSP_EXP432P401RLP_DMAControlTable[7].control =
        			(MSP_EXP432P401RLP_DMAControlTable[7].control & 0xff000000 ) |
    				(((ARRAY_LENGTH)-1)<<4) | 0x03;
        }
        else
        {
    //        MAP_DMA_setChannelControl(UDMA_ALT_SELECT | DMA_CH7_ADC14,
    //        		UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    //        MAP_DMA_setChannelTransfer(UDMA_ALT_SELECT | DMA_CH7_ADC14,
    //        		UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[0],
    //    			resultsBufferAlternate, ARRAY_LENGTH);
        	MSP_EXP432P401RLP_DMAControlTable[15].control =
        			(MSP_EXP432P401RLP_DMAControlTable[15].control & 0xff000000 ) |
    				(((ARRAY_LENGTH)-1)<<4) | 0x03;
        }
        P1->OUT &= ~BIT0;
    }
    
    void PORT1_IRQHandler(void)
    {
        P1->OUT |= BIT0;
        P1IFG &= ~BIT1;
        MAP_DMA_enableChannel(7);
        MAP_Timer_A_generatePWM(TIMER_A0_BASE, &timerA_PWM);
        P1->OUT &= ~BIT0;
    }