This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Keil MSP432 读取I/O问题

Part Number: MSP432E401Y

我用的是MSP432E401Y系列,现在只能读取到PL0的I/O,其他四个均无法读取,请问有人知道这是什么原因吗?

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
#include
#include
#include "ti/devices/msp432e4/driverlib/driverlib.h"
#include "delay.h"
#define MIN_DUTY 20
#define MID_DUTY 30
#define MAX_DUTY 40
#define GPIO_PIN_RESET 0
#define GPIO_PIN_SET 1
//#define TURN_LEFT_TIME 1100
//#define TURN_RIGHT_TIME 1100
#define TURN_SMALL 100
#define TURN_BIG 300
#define BUZZER_ON GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, GPIO_PIN_1);
#define BUZZER_OFF GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0x0);
#define READ_L2 GPIOPinRead(GPIO_PORTL_BASE, GPIO_PIN_0)
#define READ_L1 GPIOPinRead(GPIO_PORTL_BASE, GPIO_PIN_1)
#define READ_M GPIOPinRead(GPIO_PORTL_BASE, GPIO_PIN_2)
#define READ_R1 GPIOPinRead(GPIO_PORTL_BASE, GPIO_PIN_3)
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

x 出现错误。请重试或与管理员联系。