Part Number: TM4C1294KCPDT
TM4C1294KCPDTI3器件焊好后约有5%的故障率,均表现为时钟问题,会是哪些原因造成的啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294KCPDT
TM4C1294KCPDTI3器件焊好后约有5%的故障率,均表现为时钟问题,会是哪些原因造成的啊?
TM4C1294KCPDTI3R时钟异常:
CPU:TM4C1294KCPDT:
晶体:DT-26-A06Q-32.768KHz;
电容:CC41-0603-50V-10pF士5%。
软件设置为外部晶体高驱,调试了300块电路板,有18块板子时钟不走。
做了如下调试(每个步骤只做单项调整,其他条件不变):
1、用示波器测量坏板的晶体,没有振荡。
2、用示波器测量好板的晶体,有振荡。
3、将好板上的晶体更换到坏板上,故障依旧。
4、将坏板上的晶体更换到好板上,正常。(1-4步说明晶体没问题)。
5、去掉坏板上的晶体电容,故障依旧。
6、去掉好板上的晶体电容,正常。
7增大坏板体电容到20pF,故障依旧 (5-7步说明和电容没什么关系)
8、坏板软件跟踪,停在时钟检测处。
9、软件设置为内部LFIOSC,正常。
10、 去掉坏板上的晶体,外接 OSC,正常。
11、 更换坏板的CPU,正常。(目前为止,有十几块坏板子更换CPU后,均恢复正常)。