Part Number: LP-AM243
1Ch OSPI_IND_AHB_ADDR_TRIGGER_REG Indirect trigger address register 0FC4 001Ch
24h OSPI_REMAP_ADDR_REG Address remapping register 0FC4 0024h
80h OSPI_INDIRECT_TRIGGER_ADDR_RANGE_REG Indirect trigger address range register 0FC4 0080h
OSPI_REMAP_ADDR_REG,应该时内存映射地址设置,0x6000_0000
OSPI_IND_AHB_ADDR_TRIGGER_REG,应该是间接读写Flash时的触发地址
OSPI_INDIRECT_TRIGGER_ADDR_RANGE_REG,应该是间接读写Flash时的触发地址范围
按我的理解,比如我设置内存映射地址为0x6000_0000,触发地址为0x7000_1000,触发地址范围为0x1000,
那么我在读写Flash时,如果读写0x7000_1200,就可以读写Flash的0x6000_1200空间,但事实是,设置这些寄存器,没有任何反应
看TI公司官方SDK源码发现,
CSL_REG32_WR(&pReg->IND_AHB_ADDR_TRIGGER_REG, 0);
CSL_REG32_WR(&pReg->INDIRECT_TRIGGER_ADDR_RANGE_REG, OSPI_utilLog2(128));
读写Flash时,只能读写0x6000_0000,才能操作SRAM Fifo,实现间接读写功能,请专家们帮忙解释一下,谢谢