This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1227: TMS570LS1227的I2C没有停止信号

Part Number: TMS570LS1227


请教TMS570LS1227的 I2C使用问题:

1,我在pinmux中已经选择了I2C的引脚

2,在I2C配置中使能了I2C的引脚为I2C功能

3,外部有2.2K的上拉电阻,

4,发送一个字节的数据后,通过示波器监测到了,启动信号,却没有监测到结束信号,在间隔1s的时长以后,再次发送一个自己的时候,发现程序卡在了

while(i2cIsStopDetected(i2cREG1) == 0);代码处。函数的发送代码如下

void i2c_send_test(void)
{
     int32_t delay=0;
     /* Configure address of Slave to talk to */
    i2cSetSlaveAdd(i2cREG1, Slave_Address);

    /* Set direction to Transmitter */
    /* Note: Optional - It is done in Init */
    i2cSetDirection(i2cREG1, I2C_TRANSMITTER);


    /* Configure Data count */
    /* Note: Optional - It is done in Init, unless user want to change */
    i2cSetCount(i2cREG1, 1);

    /* Set mode as Master */
    i2cSetMode(i2cREG1, I2C_MASTER);

    /* Set Stop after programmed Count */
    i2cSetStop(i2cREG1);

    /* Transmit Start Condition */
    i2cSetStart(i2cREG1);

    /* Tranmit DATA_COUNT number of data in Polling mode */
    i2cSend(i2cREG1, 1, TX_Data_Master);

    /* Wait until Bus Busy is cleared */
    while(i2cIsBusBusy(i2cREG1) == true);

    /* Wait until Stop is detected */
    while(i2cIsStopDetected(i2cREG1) == 0);

    /* Clear the Stop condition */
    i2cClearSCD(i2cREG1);

    /* Simple Dealya before starting Next Block */
    /* Depends on how quick the Slave gets ready */
    for(delay=0;delay<1000000;delay++);

}

5,通过示波器抓取的波形信号如下图:

6,我通过gpio模拟I2C的程序可以正确读取从设备DS1339的数据。

求高手指点,这是什么情况,在线等...................