想要控制液晶屏,如附件所示I2C设置,这样总是调试不通过,又不知道如何检查,其中0XAA是从机地址,WriteAddr为子地址,*pBuffer为要发送的内容,想知道I2C是这样设置的吗,我看例程都是用中断进行发送的,不用中断可不可以,是不是图中代码的顺序。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,
7位从机地址应该是0xAA的高7位,0x55.
初始化也是需要对用到的管脚初始化的,可以参考下面的初始化:
//I2C
void i2cInit(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);//
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_2 | GPIO_PIN_3); //PB2---- PB3---
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE,GPIO_PIN_2);
I2CMasterEnable(I2C0_MASTER_BASE);
I2CMasterInitExpClk(I2C0_MASTER_BASE,SysCtlClockGet(),0);//I2C0 master,100kbps
}
你的数据发送代码应该是对的。